HF or UHF RFID Transponder recommendation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HF or UHF RFID Transponder recommendation

1,270 次查看
hyhaerong
Contributor I

Hello, im trying to find the RFID transponder in order to sense some analog signals

since i know that many researchers prefer NXP product because of fidelity,

really want that want to run my project with NXP products.

can you help me with finding the right model that im looking for?

 the thing im trying to find now is,

1. RFID transponder tag

2. Passive mode availability

3. Sensing interface

that is the all the features what im looking for now.

if it is possible, 900MHz frequency range might be better to use.

pic4.png

0 项奖励
回复
2 回复数

1,258 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

This one has the I2C interface.https://www.nxp.com/products/identification-security/rfid/nfc-hf/ntag/nfc-tags-for-electronics/ntag-...
And both have PWM; GPIO; I2C. https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-tags-for-electronics/ntag-5-link-nfc-forum-complian...
https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-tags-for-electronics/ntag-5-boost-nfc-forum-complia...
But the above products can't match with 900MHz frequency.
Hope it help you. Have a nice day

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复

1,253 次查看
hyhaerong
Contributor I

Really appreciate the swift response.

i totally understand that, without electrical power for the rfid transponder circuit, it is tough to achieve our goal.

 

so then, one question I have with is, when reader makes incident electromagnetic field, in order to communicate with RFID transponder,

is it possible to active (make enough power to turn on the) IC chip in the transponder by making an rectifier or something like that (pic #1)?

 

picture 1picture 1

or should we have to consider another way to solve the power consumption problem (for example battery).

 

So far, I thought the only thing I had to consider was, design of the antenna, and choosing the RFID transponder IC chip (pic #2). but seems apparently not.
Would you mind if I ask you to give me a little help to verify that your products are suitable for our purpose or not?

picture 2picture 2

 

i mean does incident field from a reader can activate the IC chip? or should i have to consider about the power consumption for the RFID transponder side as well?

0 项奖励
回复