HELP!! FS6511 FS0B pin always be low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HELP!! FS6511 FS0B pin always be low

878件の閲覧回数
snow
Contributor I

I am using the Safety Power System Basis Chip fs6511.In normal stituation,the FS0B should be high voltage.But now the FS0B always be low, and the unnormal thing is that the WD_ANSWER register FSxB bit is 0. It seems mean that there is no fail-safe event but the FS0B still be low.

pastedImage_1.png 

I have made the FS0B pin to pull-up. The faults I had configured to not impact the FS0B.

pastedImage_2.png

pastedImage_3.png

And I release the FS0B at first. But I am not sure whether FS0B should release every watchdog window.

pastedImage_5.png

This is the register that I read. FS0B is low.

pastedImage_4.png

Who can help me......

タグ(1)
0 件の賞賛
3 返答(返信)

665件の閲覧回数
flyskyr丶
Contributor III

hello,

I have the same problem.Can you tell me how to deal with it.

Thanks!

0 件の賞賛

665件の閲覧回数
flyskyr丶
Contributor III

 Now it‘s fine. Because of too large pull-up resistor .

0 件の賞賛

665件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Thanks for your interesting in NXP products.

Could you please setup a ticket with your schematic attached ASAP?

0 件の賞賛