Hi
I am using a MPC8315ERDB board. For this i've an external button which is connected to GPIO pin 7 of the board. And if this button is pressed then certain files have to be deleted. Browsing through the internet i found that GPIO drivers have to be included into the kernel and hence i set a 'y' to CONFIG_MPC8xxx_GPIO, CONFIG_GPIO_SYSFS and CONFIG_ARCH_WANT_OPTIONAL_GPIOLIB etc. And the dts file has be modified to include the following lines
gpio1: gpio-controller@c00 {
#gpio-cells = <2>;
compatible = "fsl,mpc8315-gpio", "fsl,mpc8349-gpio";
reg = <0xc00 0x100>;
interrupts = <74 0x8>;
interrupt-parent = <&ipic>;
gpio-controller; };
this is included under immr@e0000000.
further i included
erase-button@0 {
compatible = "erase-button";
interrupts = <7 2>;
interrupt-parent = <&gpio1>;
};
am i right in including this? coz after compiling the kernel i get a folder under /sys/class/gpio. I did an export using
echo 192 > /sys/class/gpio/export.
192 was the number appearing in gpiochip192/base.
It created another folder gpio192.
However i'm not able to set the value in them nor the direction.
echo 1 > /sys/class/gpio/gpio192/value
cat /sys/class/gpio/gpio192/value
returns a value of 0 only.
Am i doing it correctly? How to check it programatically if the button is pressed and take the corresponding action! Plz help!
My kernel version is 2.6.35.9.
Thanking you in advance.
已解决! 转到解答。
I fixed it myself! And some changes had to be made. The erase-button is not needed in the dts file. Further since the Gpio pin 7 needs to be controlled, the value in gpiochipN/base should be added with 7 and then the command should be given
echo N+7 > export.
Further in order to make the GPIO pin to be functional the SICRH register should be reset for GPIO pin 7 to be enabled. The bits 6 and 7 of SICRH register in 0xe0000118 should be set 1 so that the pin 7 would become functional. Thanks all if u happened to visit my post here!
I fixed it myself! And some changes had to be made. The erase-button is not needed in the dts file. Further since the Gpio pin 7 needs to be controlled, the value in gpiochipN/base should be added with 7 and then the command should be given
echo N+7 > export.
Further in order to make the GPIO pin to be functional the SICRH register should be reset for GPIO pin 7 to be enabled. The bits 6 and 7 of SICRH register in 0xe0000118 should be set 1 so that the pin 7 would become functional. Thanks all if u happened to visit my post here!