FRDM-KW019032 & FXTH870 LF Not Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW019032 & FXTH870 LF Not Working

628件の閲覧回数
swils226
Contributor II

I am trying to send LF commands from an FRDM-KW019032 transceiver board to an FXTH870 development board through the NXP GUI that is compatible with these two devices however it does not seem to be working. I have made certain that the user configuration file for the FXTH870 is set to LF however when I click the buttons on the GUI to actually send and receive info, nothing is received back by the FRDM. Is there another setting or anything that I must do in order to make this work? 

0 件の賞賛
返信
1 返信

542件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Syd,

I believe my colleague Camille has already answered this question directly by email.

If not, please let me know and I will follow up.

Best regards,

Tomas 

0 件の賞賛
返信