Design a reader Antenna for beginners

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Design a reader Antenna for beginners

402件の閲覧回数
rwerner
Contributor I

Hello

I am trying to design a reader Antenna with a range of 5cm with the PN7462AUEV.

The Problem is that i want to know the needed magnitude flux for the tag (MIFARE Classic® EV1 4K) to run.

The only Things i find in the datasheet are the Input capacitance of 16,9pF and the maximum ratings for current.

0 件の賞賛
1 返信

315件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Please kindly refer to NFC Antenna Design  for details.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛