I have downloaded RF High Power Model Kit and Product Model Design Kits of MRFE6VS25NR1 from your webpage and copied into my AWR 11 and AWR 12. Unfortunately an error that the model is 32-bit and AWR 64-bit emerge with a recommendation of using 64-bit models of components (viz. enclosed file). Is possible to get 64-bit model of the MRFE6VS25NR1 or an advice how to solve it?
Thanks.
Martin
We do not have a 64 bit model for the older devices, only the 32 bit option is available. The existing 32 bit model should work with AWR 11.
Have a great day,
Andrei
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------