Dealing with Thermal Pad of PCAL6524HEAZ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dealing with Thermal Pad of PCAL6524HEAZ

跳至解决方案
694 次查看
Edgard
Contributor III

Dear an Engineer in NXP

I have one question about the Thermal Pad of PCAL6524HEAZ.
I checked the comment that the Thermal Pad is not connected to internal chip directly.

Is it NOT necessary to connect to GND pattern on PCB with the Thermal Pad?

Thanks in advance
Edgard

0 项奖励
回复
1 解答
668 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

在原帖中查看解决方案

2 回复数
669 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eduard,

you are correct. The thermal pad underneath the PCAL6524HEAZ is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

With Best Regards,

Jozef

664 次查看
Edgard
Contributor III
Dear Jozef

thanks for your quick response.
I may connect the Thermal PAD to GND.

Kindest Regards
Edgard