DSP56F801EVM examples source!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56F801EVM examples source!

3,472 Views
ali_
Contributor I
Hello everyOne,
I’ve bought DSP56F801EVM kit for our RFID experiments, as bad things do happen! My cds (those that were with kit) are somehow misplaced. I’ve tried my best to find but no luck;-)
I have gathered docs and codeWarrior from freescale website but can’t find any code examples for DSP56F801EVM kit like one is available here [
http://www.freescale.com/faqdata/FAQ-11868-ADCSPL56F807EV.exe ]
. It would be great if somebody here can point me to the DSP56F801EVM kit examples source.


Thanks for your time.
Tags (2)
0 Kudos
Reply
3 Replies

1,054 Views
Nabla69
Contributor V
Hi,

You should probably change the way you are looking for things as a simple search using the "Enter Part Number" above returns a full page page with applications code example and all info about the board...

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DSP56F801EVM

56800CEHW
Peripheral Example Applications for 56800/E, supporting: ADC, Decoder, ESSI/SSI, EMI, Flash, GPIO, HPI, INTC, I2C, PLL, PWM, Timer, SCI/LIN, SIM, SPI, TOD, EEPROM, Terminal, Button, Codec, LED, Switch.

User Manual, Gerbers of the board....

Message Edited by Nabla69 on 2006-10-0306:38 AM

0 Kudos
Reply

1,054 Views
ali_
Contributor I
Thanks for post;-)

Doh! You are absolutely right. **bleep** I’ve seen many times “DSP56F801EVM : Evaluation Kit for 56F801 Processor” resource page as pointed by you also. But never noticed that there is a download link [ http://www.freescale.com/files/dsp/software/libraries/56800CEHW.zip ] for Code Examples on the same page.

>You should probably change the way you are looking for things.

I’d note it as a note. l0l



ali
0 Kudos
Reply

1,054 Views
ali_
Contributor I
Hello All,

X:GPIO_B_DDR = ( 1 shift_left var ) ;

Complier reports it as "Not an lvalue";-)And how can i do somthing like :

X:GPIO_B_DDR = (1 shift_left var | 1 shift_left var2 ) ;

Fourm interface don't allow me to write C Shift_Left operator;-)And what is the problem in following piece of code:

asm(move #1, X:GPIO_B_DDR); // It is OK

int some =34;

asm(move #@ABS(some), X:GPIO_B_DDR); // an ERROR here

And how about LEA? **bleep** its first time to work with DSP and even with Motorola gadgets.I’ve got the MOTOROLA DSP ASM REF Manual but can’t find any its C version.


Thanks for your time,
ali
0 Kudos
Reply