Custom Firmware image creation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Custom Firmware image creation

跳至解决方案
726 次查看
Ghouse
Contributor V

Hi, iam using LS1046ardb in a custom card, i want to change the rcw file and build the firmware image with the modified rcw file.

please provide the complete process for generating custom firmware image using modified .rcw file.

Although flex-builder -c rcw -m ls1046ardb can be used to make the "bl2_qspi.pbl",  i want to know if there a procedure to generate the firmware image using .rcw or bl2_qspi.pbl..

0 项奖励
回复
1 解答
705 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

在原帖中查看解决方案

0 项奖励
回复
1 回复
706 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

0 项奖励
回复