Could MC34844A reach 60V output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could MC34844A reach 60V output?

441 Views
jordom
Contributor I

Dear Sirs:

I would like to work with the MC34844A under the following requirements:

  • Vin = 12V
  • Vout = 60V
  • Ioutmin = 0,3A
  • Ioutmax = 0,6A
  • For dimming a 3V PWM is using with a variable frequency depending on the specific application.

Is is possible to reach such voltaje we made several tests but we never reach more than 47V and we are not sure we can fron the datasheet data.

If 60 V( and current mentioned) are reachable please let me know the values of:

L

Cout

Ccomp1

Ccomp2

Rslope

Rpcomp

Rccomp

Thanks in advance

Jorge Domingo

DFAE Freescale

EBV ELEKTRONK

0 Kudos
1 Reply

298 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Jorge,

Yes, you can reach up to 60V output with the MC34844A, but not with a VIN of 12V, you would need an input voltage of 28V (with an Iout typ of 0.4A) with the following components values:

L = 120 uH

Cout = 47 uF

Ccomp1 = 8.6 nF

Ccomp2 = 99.5 pF

Rslope = 216 Kohms

Rcomp = 5.6K


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos