Can I use old date code for MRF9045LSR1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use old date code for MRF9045LSR1

527件の閲覧回数
sakri_ahmad
Contributor I

I have MRF9045LSR1  with date code 1228, 1229 (year 2012). 

Can I use this device for my product?

ラベル(1)
  • RF

0 件の賞賛
1 返信

426件の閲覧回数
LPP
NXP Employee
NXP Employee

Yes. You can use this device.

For  NXP  devices  offered  with  a  gold lead finish,  adequate solderability is ensured in the end application. If no harmful contamination comes into contact with the components, there is no aging process in the parts and they will have a almost unlimited shelf life span.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛