Can I get the linux device driver of PCAL6524(IO Expander), or similar device??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I get the linux device driver of PCAL6524(IO Expander), or similar device??

3,637件の閲覧回数
andykim
Contributor I

I am going to use PCAL6524 at my system(Android)...

So I want to get PCAL6524 Driver, or a driver of a similar device(IO Expander) for reference.

Thanks for reading

0 件の賞賛
返信
4 返答(返信)

3,068件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello Andy,

Here it is the Linux driver for PCAL6524.

I hope this could be helpful for you.

Best regards,

Diego.

0 件の賞賛
返信

3,068件の閲覧回数
rajesh_koodal28
Contributor I

Hi Adrian,

I am using one of the I2C IO expander supported by the linux driver gpio-pca953x.c.

I have connected this io expander interrupt line to the gpio and this gpio interrupt line is connected to gic.

The gpio-pca953x.c driver interrupt handler, runs only in threaded irq, as it has to communicate over i2c.

Now, when the input of this expander is triggered, the interrupt finally is generated at the interrupt controller and my GPIO pin handler is called in the hwirq context. The GPIO pin handler is a chained irq handler which is chained to the threadedirq handler of gpio-pca953x.c.

While at the GPIO pin handler, the irq are disabled and then this handler further wakes up the threaded irq handler of the io expander and after this while returning the irq at GPIO pin are again enabled.

But the problem here is, until, we acknowledge the io expander, the output interrupt pin of the io expander will still be high. Because of this, the GPIO pin handler is again triggered and this continues to happen in hwirq context without the threaded irq handler of gpio-pca953x.c getting a chance to run and clear the output interrupt.

If i need to handle this issue, then i need to disable the GPIO pin interrupt in my GPIO pin handler and exit the hwirq, then, when the threaded irq of io expander runs, once it clears its output interrupt, it would have to then enable the GPIO pin interrupt.

To achieve this the gpio-pca953x.c doesn't provide a standard framework.

In general how are these situations handled in linux while dealing with io expander's output interrupt either connected to interrupt controller via a GPIO pin or directly to it.

please provide your inputs

0 件の賞賛
返信

3,068件の閲覧回数
andykim
Contributor I

Hello Diego,

Thanks for your reply.

I am a novice for the linux device driver.

I have read the attached file, rt122285-drad-1_1.pdf.

This file referred to linux/drivers/gpio/pcal6524.c, device driver for PCAL6524.

How can I get this source code?

I could not fine this file at attached files.

I hope your reply.

Best regards,

Andy

0 件の賞賛
返信

3,068件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello Andy,

Here you have the link for the git. Here, you could have all the needed information.

linux-upstream/scripts at emcraft · EmcraftSystems/linux-upstream · GitHub 

Also, I attached you the pcal6524.c file.

I hope this information answers your question.

Best Regards,

Diego.

0 件の賞賛
返信