Hi,
I am working on the PN7462AU card reader with Evaluation kit using PN7462AU-FW_v05.07.01_Full firmware file with "phExCcid" example. Which is for Contact and Contact-less cards detection.
I need to perform the operation on both card when both are present at same time. But yes only one card get the command fired by the user respectlivily.
For example say that, Card reader has both the card Contact and contact-less card present at the same time. When user need to fire command for contact card then it should received by contact card similarly for the contact-less also. (For Contact-less card - ISO-14443 Type A and contact card - SAM CARD).
In short I need to perform the operation on both cards (contact and contact-less cards) but one at a time in presence to two cards - contact and contact-less cards.
So, Please kindly guide to achieve these functionality for two card operation on PN7462AU.
If possible then also share the API/data/document/any example related to it.
Your all the support & response are highly appreciative.
Looking forward for the supports.
Best Regards,
Hello sir,
Unfortunately, we don't have a solution that we can provide. The examples that we have in the NFC Reader Library aren't designed for concurrent execution. This will have to be developed by your team.
I'm very sorry that we aren't able to help you with this matter.