CPU not Halted when jlink segger debug is used on Module : PN7642

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU not Halted when jlink segger debug is used on Module : PN7642

5,832件の閲覧回数
Ketul
Contributor I
 
0 件の賞賛
返信
3 返答(返信)

5,356件の閲覧回数
Parmiss
Contributor I

Hi @Ketul ,

I have the same issue with this module. Could you solve the problem?

Best regards,

Parmiss

0 件の賞賛
返信

5,830件の閲覧回数
Ketul
Contributor I

Hi All , 

 

I am not able to flash my hex file in to PN7642  using J Link segger , when try to flash I am geting error like CPU not halted , please find below log:

 

IDE : MCU EXPRESSO IDE VERSION 11.8

Jlink segger version : V7.92 

SEGGER J-Link Commander V7.92l (Compiled Oct 25 2023 15:22:50)

DLL version V7.92l, compiled Oct 25 2023 15:21:06

J-Link Command File read successfully.

Processing script file...

J-Link>ExitOnError 1

J-Link Commander will now exit on Error

J-Link :r

J-Link connection not established yet but required for command.

Connecting to J-Link via USB...O.K.

Firmware: J-Link V9 compiled May 7 2021 16:26:12

Hardware version: V9.30

J-Link uptime (since boot): N/A (Not supported by this model)

S/N: 609300836

License(s): RDI, FlashBP, FlashDL, JFlash, GDB

VTref=3.282V

Target connection not established yet but required for command.

Device "PN7642" selected.

Connecting to target via SWD

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

Scanning AP map to find all available APs

AP[1]: Stopped AP scan as end of AP map seems to be reached

AP[0]: AHB-AP (IDR: 0x84770001)

Iterating through AP map to find AHB-AP to use

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

Cortex-M (ARMv8-M and later): The connected J-Link (S/N 609300836) uses an old firmware module that does not handle I/D-cache correctly. Proper debugging functionality cannot be guaranteed if cache is enabled

FPUnit: 8 code (BP) slots and 0 literal slots

Security extension: implemented

Secure debug: disabled

CoreSight components:

ROMTbl[0] @ E00FE000

[0][0]: E00FF000 CID B105100D PID 000BB4C9 ROM Table

ROMTbl[1] @ E00FF000

[1][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33

[1][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT

[1][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB

[1][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM

[1][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM

[1][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI

[0][1]: E0045000 CID B105900D PID 004BB907 DEVARCH 00000000 DEVTYPE 21 ETB

[0][2]: E0045000 CID B105900D PID 004BB907 DEVARCH 00000000 DEVTYPE 21 ETB

[0][3]: E0044000 CID B105900D PID 002BB909 DEVARCH 00000000 DEVTYPE 22 ATBR (?)

[0][4]: E0046000 CID B105900D PID 005BB906 DEVARCH 00000000 DEVTYPE 14 CTI (?)

Memory zones:

"Default" Description: Default access mode

Cortex-M33 identified.

Reset delay: 0 ms

Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: Core did not halt after reset, trying to disable WDT.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: CPU did not halt after reset.

Reset: Using fallback: Reset pin.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Core did not halt after reset, trying to disable WDT.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Failed. Toggling reset pin and trying reset strategy again.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: Core did not halt after reset, trying to disable WDT.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: CPU did not halt after reset.

Reset: Using fallback: Reset pin.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Core did not halt after reset, trying to disable WDT.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

CPU could not be halted

****** Error: Failed to halt CPU.

J-Link>h

CPU could not be halted

J-Link>loadfile "C:\Users\40024076\Documents\MCUXpressoIDE_11.8.1_1197\workspace\pnev7642fama_NfcrdlibEx9_NTagI2C_Bm_Pub\Debug\pnev7642fama_NfcrdlibEx9_NTagI2C_Bm_Pub.hex"

'loadfile': Performing implicit reset & halt of MCU.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: Core did not halt after reset, trying to disable WDT.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: CPU did not halt after reset.

Reset: Using fallback: Reset pin.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Core did not halt after reset, trying to disable WDT.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Failed. Toggling reset pin and trying reset strategy again.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: Core did not halt after reset, trying to disable WDT.

Reset: ARMv8M core with Security Extension enabled detected.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via AIRCR.SYSRESETREQ.

Core did not halt after reset, halting it manually.

Reset: CPU did not halt after reset.

Reset: Using fallback: Reset pin.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

Reset: Core did not halt after reset, trying to disable WDT.

Reset: Halt core after reset via DEMCR.VC_CORERESET.

Reset: Reset device via reset pin

Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).

Reset: Reconnecting and manually halting CPU.

Found SW-DP with ID 0x6BA02477

DPIDR: 0x6BA02477

CoreSight SoC-400 or earlier

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FE000

CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)

Feature set: Mainline

Cache: No cache

Found Cortex-M33 r0p4, Little endian.

CPU could not be halted

CPU could not be halted

****** Error: Failed to halt CPU.

CPU could not be halted

Downloading file [C:\Users\40024076\Documents\MCUXpressoIDE_11.8.1_1197\workspace\pnev7642fama_NfcrdlibEx9_NTagI2C_Bm_Pub\Debug\pnev7642fama_NfcrdlibEx9_NTagI2C_Bm_Pub.hex]...

CPU could not be halted

CPU could not be halted

****** Error: Timeout while preparing target, RAMCode did not respond in time!

Failed to perform RAMCode-sided Prepare()

Cannot read register 16 (XPSR) while CPU is running

Cannot read register 20 (CFBP) while CPU is running

Cannot read register 0 (R0) while CPU is running

Cannot read register 1 (R1) while CPU is running

Cannot read register 2 (R2) while CPU is running

Cannot read register 3 (R3) while CPU is running

Cannot read register 4 (R4) while CPU is running

Cannot read register 5 (R5) while CPU is running

Cannot read register 6 (R6) while CPU is running

Cannot read register 7 (R7) while CPU is running

Cannot read register 8 (R8) while CPU is running

Cannot read register 9 (R9) while CPU is running

Cannot read register 10 (R10) while CPU is running

Cannot read register 11 (R11) while CPU is running

Cannot read register 12 (R12) while CPU is running

Cannot read register 14 (R14) while CPU is running

Cannot read register 15 (R15) while CPU is running

Cannot read register 17 (MSP) while CPU is running

Cannot read regi

Unspecified error -1

Script processing completed.

Unable to perform operation!

Command failed with exit code 1

 

0 件の賞賛
返信

5,790件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Ketul:

 

First you can check whether JLINK is working properly, you can try to connect it to different board and see if you can successfully program the board.

Then you can check the PN7642 EVK board,  check the jumpers are in the default position?

Also check the PN7642 firmware version, try to use the latest version and try it again.

 

Regards

Daniel

 

 

 

0 件の賞賛
返信