CD1030 switch interactions and types

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CD1030 switch interactions and types

782 Views
testbed
Contributor III

Hi,

I am planning to use the CD1030 33 channel MSDI in my project.

Just wanted to know if the following switch interactions using this chip are feasible or not

All switches are momentary-push-to-on type

Interactions

1. Long Press to trigger some functionality

2. Short press to trigger some functionality

3. Long Press + Short Press combinations.(e.g. SP0 long press + SG0 short press / SP0 long press + SP2 short press)

4. When multiple switches are pressed (unless its' the combination in [3]) no action must be taken.

I know that the IC generates an IRQ on switch state change. Therefore, for the momentary-push-to-on buttons there will be two IRQs for every press. The evaluation kits and the provided S32K project use standard switches that are SPST type which generate only one IRQ to the host processor

Regards

Tags (4)
0 Kudos
Reply
0 Replies