Hello,
I'm trying to build a Zigbee example project for a K32W061 board on an evaluation board.
I followed this tutorial : https://www.nxp.com/document/guide/getting-started-with-the-k32w061:GS-K32W061
First of all, I build a SDK : https://mcuxpresso.nxp.com/en/select?device=K32W061DK6 with the following options :
Inside the MCUXpresso IDE, I installed the SDK by doing a drag and drop of the SDK into the "Installed SDKs" view.
I want now to build a zigbee example, so I import one project from the examples :
Right-click on the projet -> Build project and I end up with this error :
Building file: ../zigbee/BDB/Source/FindAndBind/bdb_fb_common.c
../zigbee/BDB/Source/OutOfBand/bdb_DeviceCommissioning.c:38:10: fatal error: pdum_gen.h: No such file or directory
38 | #include "pdum_gen.h"
| ^~~~~~~~~~~~
compilation terminated.
I'm building with an Ubuntu system, is it the root of the error ?
When building the wireless/zigbee/coordinator bare metal example, I'm getting the same error on Windows 10 with SDK 2.6.12, fresh install of IDE and SDK, following the instructions above.
14:05:33 **** Build of configuration Debug for project jn5189dk6_zigbee_coordinator_bm ****
make -r -j8 all
sh ../tools/ZPSConfig/Source/ZPSConfig -n coordinator -f ../source/Coordinator/Source/coordinator.zpscfg -y; sh ../tools/PDUMConfig/Source/PDUMConfig -z coordinator -e LITTLE_ENDIAN_PROCESSOR -f ../source/Coordinator/Source/coordinator.zpscfg -o ../source/Coordinator/Source; sh ../tools/ZPSConfig/Source/ZPSConfig -n coordinator -t JN518x -l ../libs/libZPSNWK.a -a ../libs/libZPSAPL.a -e LITTLE_ENDIAN_PROCESSOR -f ../source/Coordinator/Source/coordinator.zpscfg -o ../source/Coordinator/Source -c "C:\NXP\MCUXpressoIDE_11.8.0_1165\ide\/tools/"
Traceback (most recent call last):
File "<stdin>", line 49, in <module>
ModuleNotFoundError: No module named 'lxml'
File "<stdin>", line 45, in <module>
ModuleNotFoundError: No module named 'lxml'
File "<stdin>", line 49, in <module>
ModuleNotFoundError: No module named 'lxml'
make[1]: [makefile:93: pre-build] Error 1 (ignored)
... much later ....
../zigbee/BDB/Source/OutOfBand/bdb_DeviceCommissioning.c:38:10: fatal error: pdum_gen.h: No such file or directory
38 | #include "pdum_gen.h"
| ^~~~~~~~~~~~
compilation terminated.
Finished building: ../zigbee/OTA/Source/OTA_ServerUpgradeManager.c
make[1]: *** [zigbee/BDB/Source/OutOfBand/subdir.mk:20: zigbee/BDB/Source/OutOfBand/bdb_DeviceCommissioning.o] Error 1
../zigbee/BDB/Source/NwkSteering/bdb_ns.c:38:10: fatal error: pdum_gen.h: No such file or directory
38 | #include "pdum_gen.h"
| ^~~~~~~~~~~~
compilation terminated.
The key here is "no module named: lxml"
You need to
install python3.x
make sure the python executable is in your PATH (set system environment variable, with the default system settings AFTER the new one for python...)
pip install lxml
restart the MCUXpresso IDE and retry the build
Hi @glecocq,
I am sorry for the late reply. I checked internally the compilation issue.
The route cause is the zps config and pdum config tools are under windows and in the Linux environment doesn't create the files that are missing on the compilation process.
Could you please use the try the Windows environment? You can use the Zigbee examples.
Sorry for any inconvenience that this may cause you.
Regards,
Mario