Bit-banged 56F8013-JTAG does not enter Select-IR-Scan state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bit-banged 56F8013-JTAG does not enter Select-IR-Scan state

2,632件の閲覧回数
MarkO
Contributor I

I am trying to bit-bang the JTAG lines of the 56f8013 with the intent of programming the flash (on another platform). I can communicate with the uP using code warrior and CCS with no problem. I can also bit-bang the JTAG port to enter the the Test-Logic_reset state and retrieve the IDCODE value. (I've verified that the ID is correct.) The problem is that if I reset the TAP, I cannot execute any JTAG instruction, e.g. IDCODE, DEBUG_REQUEST, etc. If I use CW and exit, the 56f8013 remains in a state where I, using my code, can send and receive data just fine. Is there a special sequence after the TAP resets that allows the CW code to communicate (but not my code)? BTW, I used App note 1935 "Programming On-Chip Flash Memories of 56F80X Devices Using the JTAG/OnCE Interface" as a guide.

Thanks,
Mark

ラベル(1)
  • DSC

タグ(2)
0 件の賞賛
返信
1 返信

936件の閲覧回数
DanielM
Contributor III
Hi,

have a look at FAQs in the support part of the Freescale web. Search for "flash_over_jtag_v2" (FAQ number 17920). The source code to the flash programming tool will tell you how to do this.

Daniel

Message Edited by DanielM on 2006-08-24 06:43 AM

0 件の賞賛
返信