Additional Dimension on MPN: TDA2614U

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Additional Dimension on MPN: TDA2614U

826件の閲覧回数
lourizyeoh
Contributor I

Hi, I am Louriz. I am here requesting for the additional dimension for the MPN: TDA2614U.

Based on the datasheet, it do not mentioned the dimensions for the certain portion. I have also attached the datasheet and the photo which I need dimension on. I need the information is for evaluation purpose. Would appreciated you could advised it. Thanks.

0 件の賞賛
1 返信

775件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Louriz,

 

The dimension of the “capture” image is:

Min = 0.82mm

Max = 1.035mm

image 1.jpg

 

And the dimension of the “capture 1” is not characterized and cannot be calculated with the existing data.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛