About the Voltage on SG1 pin of CD1030

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the Voltage on SG1 pin of CD1030

333 Views
todd_jhun
Contributor I

Dear all, 

I setted  SG1 pin into Wake-up Disabled.

During LPM(Low Power Mode) mode, the measured voltage on SG1 pin is about 7V. 

SG1 pin.png

I don't understnad why voltage is measured on this pin.  

How can I control to disconnect with VBATP node?

Best regards,

0 Kudos
1 Reply

281 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Todd,

In LPM, the current source is in polling mode, it is active periodic. If a SGx is set as wake-up disabled, this pin is not polling, that means the current source is not enabled on this channel. However, there would be residual voltage on this pin, the voltage on this pin may drop very slow. You can try to discharge it and measure the voltage again.

Best regards,

Tomas

0 Kudos