About iMX27 ADS(REV2.8) and WinCE6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About iMX27 ADS(REV2.8) and WinCE6.0

2,445 次查看
YJL
Contributor I
Hi
I'm trying to get the WinCE 6.0(WCE600_FINAL_MX27_SOURCE.zip) running on our iMX27 ADS board(REV2.8).
I use the WINCE6.0 to load the nk.bin to NAND flash.

But when trying to boot WINCE6, I get the Freescale on the display and
serial debug output "
WPU = 1
WPU = 2
WPU = 3
WPU = 4
WPU = 5
WPU = 6
WPU = 7
WPU = 8
OEMInterrupHandler:  No pending interrupt!
WPU = 9
WPU = 10
WPU = 11
WPU = 12
WPU = 13
WPU = 14
OEMInterrupHandler:  No pending interrupt!
WPU = 15
WPU = 16
OEMInterrupHandler:  No pending interrupt!
OEMInterrupHandler:  No pending interrupt!
OEMInterrupHandler:  No pending interrupt! "
 
Is there anything I've missed here, anyone done this successfully?
 
Thanks,
YJL
0 项奖励
2 回复数

468 次查看
YJL
Contributor I
Stop DPTC power  management, and it work.
 
Thanks all.
0 项奖励

468 次查看
MMT
Contributor I

Hi,

 

I'm using iMX27ADS eval board for design development and when I was testing for WiFi module (SDIO) on the eval board, I'm seeing the same error on the serial console. Your suggestion is to stop the DPTC power management but I have no idea how to stop this power management. Can you please further eleborate on the solution? Please advice.

 

Thanks!

0 项奖励