About CAN Wakeup Pulse in MC33742

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About CAN Wakeup Pulse in MC33742

808 次查看
vinman0261
Contributor I

Folks,

Using MC33742 (SBC - CAN Transceiver - 28 pin IC) in one of our project.

Initialized the Transceiver in Normal mode. After 100 milliseconds of Power up, CAN TX (Pin# - 2) is getting reset.

Due to this reset pulse, we couldn't able to transmit data via CAN bus. Attached the evidence for the same.

Can anyone tell me how to resolve this issue.

Thanks

Vinoth

0 项奖励
回复
2 回复数

667 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

It is being solved internally (Case 00151731).

0 项奖励
回复

668 次查看
andrea_costa
Contributor I

Hi Tomas,

i'm facing the same issue :smileysad: The SPI init sequence is the one suggested in the datasheet (DEBUG MODES WITH SOFTWARE WATCHDOG DISABLED THOUGH SPI) and i'm sending via SPI the commands  {0xB5, 0x10, 0x15, 0x5F}.

What i'm missing? How did you manage to solve the problem?

Thanks,

Andrea

0 项奖励
回复