A5G07H800W19NR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A5G07H800W19NR3

129 Views
Joey-Community
Contributor I

Dear NXP

Do you know the difference between dissipasion power and saturated power?

And what is the dissipasion power for below part?

NXPA5G07H800W19NR3
NXPA5G21H605W19NR3
NXPA5G18H610W19NR3
NXPA5G19H605W19NR3
NXPA5G08H800W19NR3
0 Kudos
Reply
1 Reply

106 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The Saturation power (Psat) is the power level achieved, even changing the input power does not produce any change in the output power level.

The dissipation power is  is the maximum allowed continuous power dissipation for a device with a mounting base at 25 C. The power dissipation is calculated as that which would take the device to the maximum allowed junction temperature while keeping the mounting base at 25 C.

The maximum rating for power dissipation (PD) is closely associated with thermal resistance (θJC). Actually maximum PD is in reality a fictitious number a kind of figure of merit because it is based on the assumption that case temperature is maintained at 25°C.

Hope this helps.

0 Kudos
Reply