12 v for driving electromagnets PCA9685

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

12 v for driving electromagnets PCA9685

544 Views
per_ottosson_gb
Contributor I
Im thinking of buying PCA9685 to control the magnetis in 16 electromagnets from raspberry pi. I intend to supply the electromagnets with 12v and connect it according to this image from adafruit. Only supply with 12 v instead of 5 v. 
https://learn.adafruit.com/assets/59271

My question is: can I feed this with 12volts external power? I am a bit confused regarding the specs. Have read a different about this. On some pages it is said that it goes up to 12 V but as far as I can see it says max 6 V in the spec.

For example here at adafruit it says:
" If you have to, you can go higher to 12VDC, but if you mess up and connect VCC to V+ you could damage your board! "

https://learn.adafruit.com/16-channel-p ... er/pinouts

Im not planning to buy it from adafruit but from europe but I guess this is exactly the same:
http://www.nxp.com/docs/en/data-sheet/PCA9685.pdf

Can I drive my magnets with 12 v connected to the external powersupply input?

Thanks
0 Kudos
Reply
1 Reply

507 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

For the PCA9685 Vdd is only support to 5.5V,about the LED output channels if you use this channel output  to control MOSFET,you can use various voltage on this external circuit to supply MOSFET.

Just as datasheet page35 showing.

0 Kudos
Reply