DC-DC converter DCM analysis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DC-DC converter DCM analysis

DC-DC converter DCM analysis

 

DC-DC converter DCM analysis

Most of time the DC-DC converter works on CCM, we also get lot of benefit from CCM high efficiency/low noise etc, usually we neglect the DCM status, in DCM we can get larger rippler/noise and low efficiency. Here we will give analysis.

guoweisun_0-1605622484445.png

 

                       BUCK converter

guoweisun_1-1605622484453.png

 

Figure2:BUCK converter in CCM inductor current iL(t),diode current iD(t)

guoweisun_2-1605622484459.png

 

Figure2:BUCK converter in DCM inductor current iL(t),diode current iD(t)

 

I>△iL in CCM ; I<△iL in DCM-----(1.3)

Where I and △iL are found assuming that the converter operates in the continuous conduction mode,we put(1.1) and (1.2) into(1.3) for get in DCM.

I=V/R------(1.1)

△iL=

guoweisun_3-1605622484459.png

 

=

guoweisun_4-1605622484460.png

 

--------(1.2)

guoweisun_5-1605622484460.png

 

<

guoweisun_6-1605622484460.png

 

Lead to

guoweisun_7-1605622484460.png

 

<D’

Which can be showed:

K<Kcrit(D)  for DCM

Where K=2L/(RTs) and Kcrit(D)=D’

guoweisun_8-1605622484466.png

 

Figure3: Buck converter Kcrit(D) vs D,converter works in CCM when K>Kcrit and in DCM when K<Kcrit

Large value of K lead to CCM,small value lead to DCM for some values of duty cycle. The critical value of K at the boundary between modes,Kcrit(D) is function of duty cycle and equal with D’ for the BUCK.

guoweisun_9-1605622484471.png

 

Figure4 Comparison of K with Kcrit(D),for a larger value of K. Since K>1,the converter operates in CCM for all D.

Figure4 shows work condition on the heavier loading,the R is reduced in value,such that K is larger,if K is greater than one ,then the converter operates in CCM for all duty cycle.

It is natural to express the mode boundary in terms of R,rather than the dimensionless parameter K, Equation(5.6)can be rearranged to directly expose the dependence of the mode boundary on the load resistance:

R<Rcrit(D) for CCM,R>Rcrit(D) for DCM where Rcrit(D)=2L/(D’Ts)

The converter enters DCM when R above the Rcrit.this critical value depends on the inductance,the switching period,and duty cycle.

Note that.since D’<=1,the minimum value of Rcrit is 2L/Ts.

Therefore,if R<2L/Ts,then the converter will operate in CCM for all duty cycle.

 

guoweisun_10-1605622484479.png

 

Figure5 CCM-DCM mode boundaries for the buck.boost and the buck-boost converters

The results are listed in Figure5 for three basic dc-dc converters.

 

 

 

In each case,the dimensionless parameters K is defined as K=2L/(RTs),and mode boundary is give by

 

 

K>Kcrit(D) or R<Rcrit(D) for CCM

 

 

K<Kcrit(D) or R>Rcrit(D) for DCM

 

 

 

无评分
版本历史
最后更新:
‎11-17-2020 07:15 AM
更新人: