kinetis M chip(MKM34Z128CLL5) support in USBDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis M chip(MKM34Z128CLL5) support in USBDM

Jump to solution
1,630 Views
kirukicosmas
Contributor I

Hello Pgo, Thank you for the great work you have done in USBDM. I have a kinetis M chip(MKM34Z128CLL5) that I am programming

on a custom board using the FRDKL25Z board and the USBDM firmware as outlined in your tutorial.However the

USBDM ARM Programmer doesn’t support that particular chip in its target list.Would suggest a solution to this?

Labels (1)
0 Kudos
Reply
1 Solution
1,122 Views
pgo
Senior Contributor V

Hi Kiruki,

Support for MKM family has been added in the last version.

It has only been tested with one device.

Let me know how it works.

bye

View solution in original post

2 Replies
1,123 Views
pgo
Senior Contributor V

Hi Kiruki,

Support for MKM family has been added in the last version.

It has only been tested with one device.

Let me know how it works.

bye

1,122 Views
kirukicosmas
Contributor I

Thank you pgo. I have successfully programmed the MKM34Z128CLL5 on the TWR-KM34Z50M board.

However, I made a custom board based on MKM33Z128CLH5(same family as the MKM34 and is supported in your latest version of USBDM) and

I have not managed to program it. I get the following errors:

The device is secured and it prompts that I do a mass erase. When I agree to unsecure and mass erase the device, I get:

Unsecuring the device failed.

Reason:Execution of TCL script returned an error.

Please point me in the direction I can take to resolve the errror.

Thanks.

0 Kudos
Reply