clock trimming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

clock trimming

3,017 次查看
elruocch
Contributor I
Hello all,
I would like to know if the clock trimming capability in the CW is supported using OSBDM08.
Thanks in advance
Andrea
 
标记 (2)
0 项奖励
3 回复数

369 次查看
peg
Senior Contributor IV
Hello and welcome elruocch,

Unfortunately the OSBDM does not support automatic calculation of the required trim value for internal clock generators.
You can refer to AN2312, AN2496 and AN2498 for help with this.


0 项奖励

369 次查看
elruocch
Contributor I
Thank you Peg,
I've checked the ANs.
Do you think that it would be possible to add the trimming feature? I mean, supposing no problem in modifying the firmware, how does the CW manage this option? Could the dll be modified? Or is the command already implemented?
regards
Andrea
 
0 项奖励

369 次查看
peg
Senior Contributor IV
Hi,

AFAIK most of the work for working out the trim is done by the BDM adapter (P&E USB Multilink for example). It needs to measure the response from the target with sufficient accuracy in the first place though. This, I believe is where the problem is with OSBDM/TBDML et al.

0 项奖励