On a previous occasion my JS16 USBDM was not recognised. On advice from pgo I checked the "device instance", which was USB\VID_15A2&PID_0038\... - showing it to be in ICP mode. I re-booted the unit using the JS16 BOOTLOADER and then everything worked fine. Yesterday I moved it to another PC with new app and driver installation and it showed up on the interface tab of the HCS08 Programmer. Today it was not recognised by the HCS08 Programmer so I repeated the process. Sure enough, it was in ICP mode, so I re-booted it, which completed successfully (or so it said). Result - Nothing. One device shown in the device manager as "Working Correctly", but not recognised by The HCS08 Programmer or the USBDM Firmware Updater. Unfortunately I do not have access to the original PC. Any ideas?
I moved this thread to OSBDM and TBDML space, thus the USBDM expert can see it.
Best Regards,
Jennie Zhang