USBDM can´t program PA16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USBDM can´t program PA16

跳至解决方案
1,983 次查看
lucianonicolau
Contributor III

Hi pgo,

Using 4.10.6.140 I have MC9S08PA16 on my board and it only can be programmed if selected as PT16.

If selected the right device "PA16" it cause this error:

usbdm_problem.jpg

Tell me how to fix it.

thanks!

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,641 次查看
pgo
Senior Contributor V

Hi Luciano,

The manual for the chip indicates that the SDID is 0x0042 so it looks like the first digit is the mask revision.

I've changed the SDIDmask in the attached file which should have the same effect as the changes you made but also work with the version given in the manual.

I would appreciate it you could test this.

I have previously added your site to the list on:

http://usbdm.sourceforge.net/

bye

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,641 次查看
pgo
Senior Contributor V

Hi Luciano,

I've attached an updated hcs08_devices.xml file.  Can you replace this file in the USBDM installation and check if it works correctly with your devices.

Place in directory C:\Program Files (x86)\pgo\USBDM 4.10.6.170\DeviceData

If this doesn't work correctly could you provide the ID number that the programmer detects?

bye

0 项奖励
回复
1,641 次查看
lucianonicolau
Contributor III

Hi pgo,

First test it stop working for PT16 too, then I changed the SDID and it works fine!

The SDID for PA8 and PA16 is 1042 (tested for both), I edited your new hcs_device.xml, now it can detect chip for PA8 and PA16.

See file attached with new SDIDs.

When you have time, please, insert my website on USBDM website as manufacturer: www.usbdm.com.br

thanks a lot,

0 项奖励
回复
1,642 次查看
pgo
Senior Contributor V

Hi Luciano,

The manual for the chip indicates that the SDID is 0x0042 so it looks like the first digit is the mask revision.

I've changed the SDIDmask in the attached file which should have the same effect as the changes you made but also work with the version given in the manual.

I would appreciate it you could test this.

I have previously added your site to the list on:

http://usbdm.sourceforge.net/

bye

0 项奖励
回复
1,641 次查看
lucianonicolau
Contributor III

I tested and it works perfectly!

thank you pgo !

0 项奖励
回复