USBDM can't be used in freescale KSDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM can't be used in freescale KSDK

1,129件の閲覧回数
wangbaode
Contributor IV

hi pgo,

I want to use usbdm to debug demo in ksdk. but i'm failed. the error is in the picture.

bye

タグ(3)
0 件の賞賛
返信
4 返答(返信)

901件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

Have you updated the firmware to the version included with USBDM?

This looks like a problem with it expecting a different response on register read failure.

bye

0 件の賞賛
返信

901件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

According to your response , I update the firmware and retry it . but It's failed to debug ksdk project . If i new a project in kds , usbdm can debug the projcet .

you can download the freescale sdk from the link and try it.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK&fsrch=1&sr=8&pageNum=%E4%...

0 件の賞賛
返信

901件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

I don't have a twrk60d100 to try out your example, however I was able to load several of the other demonstrations for other boards without significant problems.

When I tried the flash_demo_twrk60d100m example with a TWR-K60N512 it did load but did not execute correctly as it is the wrong CPU.

bye

0 件の賞賛
返信

901件の閲覧回数
wangbaode
Contributor IV

OK,thank you

0 件の賞賛
返信