Dear All,
The latest version of the hardware/software & firmware for the above is available at this location.
http://opax.swin.edu.au/~3340694/USBDM/USBDM/html/
History
Please note that these design are different from the Freescale OSBDM-JM60 design which was proceeding independently while I was doing the above designs.
Linux files will be uploaded in the next few days.
Its a BETA because there have been lots of changes in how it operates so probably some undiscovered bugs.
Enjoy.
bye
Hi there, do you know where could I buy a USBDM programmer for MCF5223X: Integrated ColdFire V2 micro?
I found here
http://usbdm.sourceforge.net/USBDM_V4.6/USBDM_CF_JMxx/html/index.html
a possible pcb, but I do not know where to buy the pcb or the assembled device ... thank you in advance,
Maurice
Dear joncas,
I've been playing with programming the STM arm devices (STM32F family). They use the older ARM connector (0.1" spacing). The newer devices use the half-pitch version used with kinetis devices. They are also less risky to play with than the Kinetis devices - no possibility of permanently securing them if I make a mistake.
Basically it was added just in case. There may be no significant support for other devices.
There will be a updated (compatible) version of the hardware with the next release.
bye
Dear Mickey,
I tested the DSC drivers last week (honest!)
Since then I stuffed up copying files between Linux and Win32.
Both the DSC firmware and drivers need to updated from the new ones on sourceforge.
Let me know how these work.
bye
Hi,
I have built the USBDM programmer with JS16 CPU and I can't download the FW.
My sequential steps are:
- short the BL signal (pin7 of MC9S08JS16) to ground
- connect the USBDM to USB
- WIN_XP reconnects the device and prompts "JS16"
- When trying to download the FW with "Bootloader JS Family GUI" whit AUTO command the Status Window show "The JM60 is not Connected or is Not in a Bootloader Mode."
Can anyone help me?
Thanks in advance
Alberto.
Dear Alberto,
The sequence you followed appears correct so there isn't much to suggest.
Could you check that the device appears correctly in the Hardware Manager. It should appear as Freescale JS family Bootloader. If it doesn't appear it is likely there is something wrong with the hardware. If it appears but under a different description (e.g. unknown device or even libusb device) then the driver is wrong and should be re-installed. Note the required driver is in the Freescale GUI application directory - C:\Program Files\Freescale\JS16 USB Driver\Automatic Bootloader USB Driver. It can be changed using the right-click menu in the hardware manager.
bye
Dear PGO!
Thank You for great work!
I try using USBDM standalone programer for HCS12 to program my board with MC9S12DP512.
The hardware is USBDM JS16 with latest version of drivers and the firmware.
The "trouble" is - I don't have possibility to load .s19 file with Standalone programmer. The code is approx 330 k . The displayed error is "S-record address too large". In this case loading and debuging code in CW ( Hiwave ) is without problem with same hardware, drivers and firmware.
bendjy
Dear Bluehacker,
I don't know what the difference is between a JS16 and a JS16L. They both link to the same reference manual on the Freescale site so I supect they are just different grades of the same chip e.g. Temperature range, burn in process (medical perhaps?) If this is the case then I would expect them to work identically. Another reason to think this is that there is no separate device selection for the JS16L in the Codewarrior tools.
bye
JS16L has USB bootloader support at 3.3V.
From the datasheet:
"The only difference between MC9S08JS16/MC9S08JS8 and
MC9S08JS16L/MC9S08JS8L is that MC9S08JS16 and MC9S08JS8
support USB bootloader function with voltage above 3.9 V while
MC9S08JS16L and MC9S08JS8L support USB bootloader function at 3.3 V.
Disable internal USB voltage regulator and apply 3.3 V to the VUSB33 pin
when using MC9S08JS16L and MC9S08JS8L for the USB bootloader
function."
Bill
Dear All,
I wanted to share my experiences with installing the USBDM 4.3 on Codewarrior 10 (Eclipse) for Linux, on 64-bit Ubuntu 10.10.
After an initial hiccup where I couldn't run the Codewarrior install script (CW 10 on 64-bit Ubuntu), everything ran smoothly (for a while). When I had a problem whereby the CW Eclipse IDE would terminate immediately after it loaded, I solved it by removing the P&E plugins in the Eclipse Plugins directory.
Installing USBDM on Linux
This was a simple case of running:
sudo ./Install_USBDM
from the Linux installation archive.
Installing 32-bit libraries for USBDM
My next problem was that whenever I ran any of the USBDM utilities, the utility would fail with a missing dependency (starting with libwx..._richedit.so..., etc). Fortunately, a quick Google search found:
32-bit and 64-bit: https://help.ubuntu.com/community/32bit_and_64bit and
getlibs: Automatically solves dependencies for 32-bit programs on 64-bit
Running getlibs on the USBDM "HCS08_FlashProgrammer", for example, enabled getlibs to fetch the 32-bit wxWidgets libraries required. After this, all the utlities and libraries (except for TestUSBDM, which was built against wxWidget debug libraries, which getlibs could not resolve) load and run as advertised in the USBDM documentation.
Installing USBDM as a debug configuration in CW 10
Just follow the instructions in the USBDM documentation.
Upgrading the firmware
I currently use a USBDM of my own[1], implemented on a JB16. Since there wasn't a *.abs.s19 for the JB16 in the USBDM_Flash_Images_4_3.zip archive, I used the USBDM_JB16.s19 binary from the USBDM_JB16_V4_3(10_12_08).zip archive.
I had to use a Windows machine to run the Freescale ICP programmer to upgrade the firmware.
Testing
So far I have successfully programmed and debugged against the HCS08 QD4 and the RS08 KA8.
[1] MDa01 - USBDM