Dear All,
USBDM has been updated to V4.8.
Please post any queries on this version in this thread,
Information available at: http://usbdm.sourceforge.net/
bye
Notes
V4 Revision History
Dear PGO
I have used your USBDM_CF_JMxxCLD_V3 to program the Kinetis device. But I found that the USBDM can not supply power to target,the phenomenon is that the USBDM seemed to reset itself automatictly when it tried to supply power to target,it could program only if I supply an extra power to the target.
To check my hypothesis,without the extra power,I measured the pin of JM60 which connected to MIC2026,the voltage was always low! It means that there's no signal to open the module of Target Vdd Supply.
I am so curious about this ,could you kindly give me some explanation please?
Sincerely
Admirer
Hello Newbee,
maybe there is a problem with your hardware on the usbdm board or on the target (if it has too high a current consumption), because I just completed a new layout, and the power supply to Kinetis targets works fine (you can see the photo at www.flashgenie.net )
best regards,
Robert
Dear Newbie,
Is the BDM actually resetting? If so then the USB connection would be lost. Is this occurring?
By this I mean – If you use the stand-alone programmer what error do you get. If it complains about target power then it’s not resetting. If it complains about USB communication then a reset may be occurring.
Possible reasons:
#1 – Actual reset with loss of BDM communication. The bypass capacitor on the power switch is too small or routing is causing switching currents to be seen by the JM60. This current is usually limited by the series polyfuse though I’m not sure if it is fast acting enough. It is also affected by the size of the bypass/supply capacitors on the target. It is also possible that the USB port on the PC is being temporarily overloaded by the surge. The power switch is also meant to limit surges so it would be surprising.
Solutions? Increase capacitor across power switch. Increase capacitors across MCU.
#2 – BDM complains about no target power. As a safety measure the BDM measures the target voltage a short time after turning the power on. This is meant to detect overloads at switch on. If it finds that the power hasn’t risen it turns it off again. It is possible that the delay is too short. This is also greatly affected by the target bypass capacitors. Another possibility is there is a fault with the connection for measuring the voltage which would have the same result.
Solutions? I could make this time longer or changeable.
I would appreciate if you could clarify which of the above is occurring.
bye
Dear PGO,
I am trying to recompile USBDM_JMxxCLD_V4 with the serial port enabled, but the resulting flash image has some flag set wrong and comes out for the usbdm-twr-kinetis instead.
I saw that you had posted the corrected flashimage in an update for that reason, but could you explain what needs to be done to correct the flag(s) in the project settings to be able to compile this with the serial port enabled?
(I have to confess that I have a lot of trouble getting the hang of CW 10, so haven't been able to figure this out!)
Many thanks!
Robert
Dear Joncas,
I will be releasing V4.9 shortly and will upload the corrected files. This would be a better place to start.
The correction was defining a #define symbol in the build settings undex C compiler which controls the build. Similar to:
-DTARGET_HARDWARE=H_USBDM_JMxxCLD
The permitted values are defined in the configure.h.
I can't remember which one was incorrect.
bye
Hi,
I made my own USBDM version, that will be used only for programming DSC MC56F800x. But as I needed external power to my board, I thought it would be nice to have this power provided by the USBDM. So, I used USBDM CF JS16CWJ v1.2 without all the Coldfire and BDM connectors and circuits and added TVS protections to the USB and JTAG connector (as in USBDM CF JMxxCLD v3.1) and a power source selectable between 3V3 or 5V through a pin header connector.
The problem is that I can't program anything. Initially, I used CodeWarrior Special Edition v8.3 to program the LED LAB program for MC56F8006DEMO, but CW hangs while trying to connect to USBDM and only works when I unplug it from USB.
So I tried the 56800E Flash Programmer and the same thing happened: the program hangs until I disconnect from USB and when I plug it back, windows don't manage to communicate with USBDM.
How can I know what problem is this? Is there some log the problem is described?
I'm currently using Windows 7 x64 and USBDM 4.8.
Regards,
Bruno
Dear Brunolalb,
I'm sorry but I can't suggest anything from your description.
If you want to create a log file setup as for the original description but use the following DLL:
usbdm-dsc-gdi-legacy-debug.dll
This will produce a log file in the %APPDATA%/usbdm directory.
bye
Dear PGO,
I haved installed USBDM-Version 4.8,
But I use Bootloader for update the firmware of the FlashImage file USBDM_JMxxCLD_V4.sx , it's error.
"Image file does not appear to be for this Hareware."
Why?
OPPS!
The firmware file(s) must have the wrong names. The one you are loading is intended for a Kinetis board. I'll check and re-upload the files separately to sourceforge when I work out what's gone wrong.
In the mean time you can use the V4.7 firmware. There is no significant changes.
Sorry for the confusion.
bye
Hi pgo,
I trying to use the USBDM with CodeWarrior - ColdFire V7.1
Try to add it to CodeWarrior Flash Programmer
In the manual (V4.7)
http://usbdm.sourceforge.net/USBDM_V4.8/USBDM_CF_JMxx/html/configuring_c_f_vx_page.html
Wrote that how to add USBDM to CodeWarrior as new connection (USBDM_Coldfire) and need the file -
usbdm-cfvx-gdi-legacy.dll
I can't find this file
Am I missing something ?
Error screens attached
Regards,
Mayer
Dear Mayer,
The first message indicates it can't find the wxWidgets DLL and you have indicated that you can't find the usbdm-cfvx-gdi-legacy.dll so I'm a bit confused.
You refer to V4.7 in your posting. USBDM 4.7 has been replaced by V4.8 and I can only (conveniently) do tests with the current version so the only advice I can give will relate to V4.8. If you haven't updated please do so as follows:
The installation should install all the required files for Coldfire V7.1 and you should be able to set up the interface as in the instructions you have mentioned,
You can try this with V4.7 if you really want.
bye
Dear Pgo,
Thanks for your help
Now I succeed to Erase + Program + Debug my Internal Flash memory - MCU - MCF52259
(Just for your reference - also succeed to program MC9S12A32)
Now I have another board based on MCU MCF5329 that have no Internal flash memory
We working with external Flash memory - 16MB Flash Memory js28f128p30b85 -- Intel
What I need to do to make USBDM to Erase + Program + Debug MCF5329 MCU
Through the Codewarrior Flash programmer or Through your application ColdFire V2,3,4 Programmer
What is the whole proccess to Program and debug an External Flash memory ?
Which files\algorithms I need or I can use PEmicro files ?
All Best,
Mayer
Dear Mayer,
The USBDM programmers only support programming internal flash and a limited range of types of flash at that. There is no reason why they couldn't be extended to do so but I don't have the time.
To program external flash it would be necessary to create the following:
The software is not compatible with the P&E files. There would be issues in making it so since it's distributed a GPL and P&E would rightly object!
It should however be possible to program devices use the Codewarrior software - Either V7.2 or V10.1 using the programming support built-in. I have no idea if they support the Flash you have indicated.
bye
dear pgo
today, I use "USBDM_CF_JMxxCLD v4.8" programming another "USBDM_JMxxCLC dongle", some problems, USB and cann't be properly identified, and even cause the USB crash.
I use JM16 chip, in order to solve this problem, I also use CYCLONE PRO, the same as programming program, but it's no problem, any suggestions? some address in the program contect is not the same.
Let me question, the HW USBDM_CF_JM60 version 4.6 is identicall with version 4.8.So can I flash new driver to the HW v.44.6?
Then can sb advise me how to flash driver "USBDM_CF_JMxxCLD_V4.abs.s19" to target device. After running flash programer in CW v10.1 I obtained the message
fl::target -lc "pokus"
fl::target -b 0xb0 0xfd0
fl::target -v off -l off -ie on -i "" -p
Error: missing value for option -p
and flashing is aborted, I tried to find where is setting "p" located, but unsuucessfully. Thanks beforehand for any advice.