Dear All,
USBDM has been updated to V4.6. This version adds support for Kinetis devices but please be aware that this has had minimal testing due to lack of devices to test with .
Please post any queries on this version in this thread,
Information available at: http://usbdm.sourceforge.net/
bye
Notes
Please note that these design are different from the Freescale OSBDM-JM60 design which was proceeding independently while I was doing the above designs
Hello PGO,
I just tried your version 4.6 with Codewarrior 10.1 on a clean install of Ubuntu 11.04 (32 bit).
In case it helps anyone else trying this, it required adding the following libraries with the Synaptic Package Manager:
Then it seems to run fine.
Many thanks and best regards!
Robert
Thanks Jim and pgo!
With your help and some project settings change I managed to build a 64-b version of the V4.5 shared library and the GDI.
I am still having some issues with the standalone flasher and the CW plugins though.
I was able to build the flasher with a hand made makefile.
I'll keep you updated on the progress
thanks again
I finally managed to compile everything (except the java stuff which still does not compile properly) on debian.
I can run the standalone flashers without any issues.
CW still refuses to work though. When I attempt to launch I get a generic error without any explanation.
How do I debug what is wrong?
I run ldd on the gdi.so to make sure there are no issues with the shared libraries but beside that I really have no idea what ewlse to try.
Dear Gorlik,
I'm not sure how you can run the GDI part without having the Java plugin working - or are you using the supplied versions?
If you compile the DLLs with logging enabled you should have messages from when the DLL is loaded. If the loading is failing check the exported symbols from the GDI DLLs to see if they are correct against the provided DLLs.
bye
Hi pgo!
I want to program MC13213 with standalone programmer "HCS08_FlashProgrammer.exe" with JS16 hardware and v.4.6.
This is not possible.
I got "Programming Error: Programming of target flash failed! Reason: Failed to read from target"
In this time programming with HiWave and same hardware is without problems.
After I downgrade to the version 4.5 All is OK.
We have any idea about this situation.
And another question: It is possible to read flash and save S19 file with standalone programmer
10x for great work on USBDM.
bendjy
Dear Benjy,
I tried programming a small project to a MC13213 chip using a JS16 USBDM (V4.6) and didn't have any problems. If it's working OK with V4.5 for you then stick with that for the moment. I would you appreciate checking again when the next version is available and letting know if the problem persists and I will spend more time investigating it.
bye
I can at least partly answer that one. If it is a native build, it is not CW eclipse, it is Eclipse CDT.
Hi!!!, Thanks for the help for use Freescale microcontroller.
I like know about a guide for the installation or step to step for installing.
Thank for you help!!!