Attached is version 2 of the JS16/JM16/32/60 version of USBDM.
This includes the following hardware versions:
If you want a simple BDM then I recommend the JS16. This has all the advantages of the previous JB16 version of OSBDM (ability to be programmed over USB & convenient SOIC package) as well as being USB2 Full speed. It is also available as a sample from Freescale
If you want a full-featured BDM then I recommend the JMxx version.
BDM Firmware History
ToDo list
Hello pgo, can you send or link for the altium PCB file for the below version
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JS16/html/index.html.
I am making pcb for some other project so i can paste the design with my project and send for single manufacturing.
with regards
thiag
Hello,I;m a Chinese user,who is just a rookie.I have read a lot about the JS16 description,but I can't find any file that I need to have my JS16 BDM work.So how and where can I find the files?And,what's better,can I find illustrations for the steps to deal with this?Thanks a lot.
Dear pgo,
My mcu and platdom is MC9S08JM32CLD. Using firmware is USBDM - Version 2 (JS16/JMxx Versions),but it don't connect with target board. I find the error is in bdm_enableBDM function by P&E debugging ,because return value of bdm_enableBDM is error code of BDM_RC_BDM_EN_FAILED. bdm_enableBDM function call bdm_readBDMStatus and writeBDMControl. In the bdm_enableBDM function the call order is bdm_readBDMStatus ,writeBDMControl,bdm_readBDMStatus.Value got is 2 when the first call bdm_readBDMStatus, however Value got is 2 when the second call bdm_readBDMStatus. The condition should be error ,but i don't know why.
I'm sorry for my poor english.
Hope pgo help me ,thank you !
Look forward to your reply.
Hello pgo!
A customer wants to use the OSBDM to build a stand-alone programming tool, the idea is very simple:
- the hardware would be very similar (if not identical) to the OSBDM.
- on the firmware side, we would need to change the loading algorithm to read the s19 file from internal memory
- we would need to add the target device firmware (maximum of 16K) inside the JM60, probably as a data table
Do you see major issues with this idea?
Have you seem a similar application?
Thanks!
Bruno
Dear Bruno,
You would have to consider the following points:
It would certainly be doable but a fair amount of work.
bye
Hi, I build the hardware of the programmer. When I plug into the PC, the PC recognizes the target . I´m ran the program ZADIG to install the USB drivers, and there´s no problems with that.
The problem appears when I run the Bootloader GUI to program the initial firmware in the JS16. A message appears " The JM60 is not Connected or is Not in a Bootloader Mode" , note that I´m tie to ground the pin BLMS , but I can´t program the target. Can you help me ?? Which can be the problem ???
Tanks you very much.
Javier
Dear Javier,
The driver required to program the JS16 is the one provided by Freescale with their GUI bootloader. The driver you have installed is the one required for the BDM after programming when it appears as a different device.
Please use the hardware manager to uninstall the device. Then unplug and plug in again. You should then be able to follow the instructions on this page:
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_JS16/html/installation_page.html
Good luck!
bye
Hi again pgo. Thanks for you quickly answer. I knew the web page you showed me. But I have a problem yet.
I´m did the uninstalation of the drivers like you said. Then I´m installed again with the drivers provides by the bootloader GUI .
The instalation was successful.
And now I open the program "Bootloader JS Family GUI" to install the firmware but appears the same messaje " The JM60 is not connected or is Not in a Bootloader Mode". Why is this message ?? Help me please.
Dear Javier,
Not much to suggest. I've had no problems with the bootloader.
Please check the following:
Does the device now appear correctly in the hardware manager? See attached image
If not uninstall and try installing again. Keep the BLMS pin low just in case the device isn't blank.
If the device appears then I can't think of any reason it wouldn't be detected by the bootloader.
I can only suggest trying another PC.
bye
Hi pgo I have other problem. The debug board works perfect I think. But I want to program a microcontroller JS16 so I downloaded the IDE Code Warrior Eclipse v10.0, because I understand that the Code Warrior v6.3 is don´t works with this debuger.
The problem is in the Projet Wizard because I don´t have the choose USBDM. I have only six chooses :
P&E Full Chip simulation
P&E USB BDM Multilink
P&E Ciclone Pro serial
P&E Ciclone Pro USB
P&E Ciclone Pro TCP/IP
Open source BDM
tell me what I have to do please. Thanks
Dear Javier,
Make sure you have run the following batch files in the USBDM installation files (and check for errors):
run"Install Codewarrior Files.cmd" to install the drivers
run "Install Codewarrior Wizards.cmd" to add USBDM to the Codewarrior Eclipse wizards .
Providing Codewarrior is installed to the usual location this should add the USBDM item that is missing.
If this doesn't work try running :
"c:\Program Files\Freescale\CW MCU v10.0\eclipse\cwide.exe" -clean
from a command line to tell Eclipse to refresh its settings.
USBDM supports JS16 on Codewarrior V6.x and V10.x so it should work in either.
bye
Hi pgo. I´m did the things that you saids and it´s work only in Code Warrior v10.0, the USBDM is appears. But in the Code Warrior v6.3 is not. The two programs are in the instalation folder C:\Programs Files\Freescale........
What can I do to have the option USBDM in Code Warrior v6.3 ??? because I prefer that version. I give you a picture showing my options. Thank you very much for youe help, you always help me.
Dear Javiere,
The USBDM pretends to be either a TBDML (for HCS12) or a OSBDM (for HCS08 & CFV1) in the Legacy Codewarrior versions. Choose the interface accordingly.
Refer to top of this page:
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_JS16/html/usage_page.html
bye
Dear pgo:
When I try to program my target in Code Warrior v6.3, after the USBDM Configuration, a error message appears. I give you a picture. Do you know what it´s can be ????
Hi pgo, now the debugger is working good. Thanks very much. T think I won't bother you any more, jaja, bye.
Dear Javier,
I'm glad you have got it working.
If you find that that Codewarrior gives you a message about the device being secured it is probably worth trying the stand-alone USBDM programmer to check if the device is unsecured and OK.
bye
Hello Pgo,
Can you tell difference between USBDM_CF_JMxx and USBDM_CF_JS16, interms of the Coldfire connector and BDM connectors and technical performance and since USBDM_CF_JS16 is having the connectors for Coldfire V1 to V4 and BDM
why we need to build USBDM_CF_JMxx ??? as USBDM_CF_JS16 having same connectors ??
References:
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JMxx/html/index.html
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JS16/html/index.html
with regards
thiag
Dear Thiag,
The links you posted clear describe the differences
CF_JMxx supports RS08,HCS12,HCS08,CFV1 + CFV2,3,4, DSC (and eventually Kinetis)
CF_JS16 supports CFV2,3,4, DSC (and eventually Kinetis) only
bye
Hello pgo, can you send or link for the altium PCB file for the below version
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JS16/html/index.html.
I am making pcb for some other project so i can paste the design with my project and send for single manufacturing.
with regards
thiag