USBDM (JB16 Version) V4.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM (JB16 Version) V4.9

652件の閲覧回数
GordonD
Contributor IV

All,

At the following SourceForge page: USBDM (JB16 Version): USBDM (combined TBDML/OSBDM code) for JB16

is the description of the TBDML/OSBDM code for, I assume, the HC08JB16. However, I cannot find any links to the source code on the page. Can anyone direct me to the source code for this project? If it is no longer available, are there any other versions available that can be configured to run on the HC08JB16.

Thanks in advance.

Best Regards,

Gordon

0 件の賞賛
1 返信

231件の閲覧回数
pgo
Senior Contributor V

Hi Gordon,

The latest published is at:

USBDM - Browse /Version 4.10.3/Source at SourceForge.net

There have not been any changes since then in the JB16 code.

Note: I have been informed (indirectly) that there are some problem with the JB16 code with the current version of the USBDM.  I have yet to look at this.

bye

0 件の賞賛