Hello,
I would like to intall USBDM JMx v 4.4 under Codewarrior Eclipse 10.1, Windows 7 64bit. I tried to follow instructions at http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JMxx/html/eclipse_v10_1__usage_page.html, but I cant see "USBDM" option in the Connections window. How to add USBDM to Eclipse?
Thank you
Martin
已解决! 转到解答。
Hi,
Try this from the installation instructions on site:
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JMxx/html/installation_page.html
Install Codewarrior Wizards.cmd
will modify the Codewarrior installation to add the missing settings. This file makes similar assumptions about the Codewarrior installation locations so should be checked before running.
If, after running the above command file, USBDM does not appear as an option in Codewarrior V10 it may be necessary to tell Eclipse to re-read its configuration files by using the following command (Type it at a command prompt - change the path if necessary)
"c:\Program Files\Freescale\CW MCU v10.0\eclipse\cwide.exe" -clean"
It's worked for me.
Gabriel.
Dear JimDon,
I changed line in the "Install Codewarrior Files.cmd"
set WIZARD_FILE=%ECLIPSE_PLUGIN%\com.freescale.mcu.projectwizard_1.1.8.FSL_b02015-B10\plugin.xml
to
set WIZARD_FILE=%ECLIPSE_PLUGIN%\com.freescale.mcu.projectwizard_1.3.44.FSL_b02052\plugin.xml
(because the first directory doesn't exist)
I run "Install Codewarrior Files.cmd" as Administrator, no errors.
I restarted CodeWarrior Eclipse, but still can't see USBDM option in Connections.
Hi,
Try this from the installation instructions on site:
http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JMxx/html/installation_page.html
Install Codewarrior Wizards.cmd
will modify the Codewarrior installation to add the missing settings. This file makes similar assumptions about the Codewarrior installation locations so should be checked before running.
If, after running the above command file, USBDM does not appear as an option in Codewarrior V10 it may be necessary to tell Eclipse to re-read its configuration files by using the following command (Type it at a command prompt - change the path if necessary)
"c:\Program Files\Freescale\CW MCU v10.0\eclipse\cwide.exe" -clean"
It's worked for me.
Gabriel.
Actually, there was no problem. I missed the information about running "Install Codewarrior Wizards.cmd" (see Gabriel's post).
This works only with USBDM 4.5 as USBDM 4.4 doesn't contain file "Install Codewarrior Wizards.cmd" (at least I couldn't find it) . But no problem for me, I just downloaded newer version.
Dear Gaminn,
Just to explain the absence of the "Install Codewarrior Wizards.cmd" in V4.4. The steps this command does are included in the Install command file in V4.4. It was more logical to separate it in V4.5
Also 4.4 did not support V10.1 Eclipse.
bye
Dear Gaminn,
I'm glad to help you on this forum that I follow a few years.
What I meant that worked for me was the command line to force eclipse to reread the configuration files.
"c:\Program Files\Freescale\CW MCU v10.0\eclipse\cwide.exe" -clean
Only after doing this that the USBDM appeared in the Codewarrior connections with Windows XP Professional SP3.
Here is a new twist.
I did an update to CW 10.1 because certain things were not working.
Goodby USBDM.
You have to re-run the install with :
set WIZARD_FILE_DIR=%ECLIPSE_PLUGIN%\com.freescale.mcu.projectwizard_1.3.46.FSL_b02057
and then do the clean.