Typical BDM waveform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Typical BDM waveform

2,772 Views
pblet
Contributor I
Hi,
 
I just build a OSBDM board based on the version without the RS support.
I uploaded the firmware. He his reconised by Hiware. But when I connect to my target self-made
based on a AW32 I got this message :
 
No Link To Target
 
As the OSBDM is new and my target as well, I'm not sure which one causing the problem.
 
In the file attached you can see the BDM signal (Top) and the Reset Signal (Bottom) that I have.
Has someone a working time diagram of what I should have on a normal case, just to understand
maybe where the problem is.
 
Many thanks in avance for any help
 
pblet
 
Message Edited by t.dowe on 2009-10-26 05:20 PM
Tags (2)
0 Kudos
1 Reply

486 Views
pblet
Contributor I
In Fact I have more questions :
 
1) On the target the AW32 has no XTal on board. It use the internal oscillator. Is this compatible with the OSBDM ? Or should I add an external XTal ?
 
2) It is a way to check that the AW60 is running whith the internal oscillator ?
 
3) If I have the same voltage level both on the OSBDM and the target, can I connect directly the BDM and Reset signals without the 74LVC1T45 ?
 
4) Has someone already tested the level shifter MAX 3373E from Maxim is this part usable in case of the OSBDM. ? the difference to the 74LVC1T45 is that this part need no DIR pin.
 
Best regards
pblet

Message Edited by pblet on 2007-02-0711:39 PM

0 Kudos