Slow download for Cyclone Max in CodeWarrior 10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow download for Cyclone Max in CodeWarrior 10.4

706 Views
davidfindlay
Contributor III

I am experiencing an issue with the Cyclone Max(7.76) in CodeWarrior 10.4. I am using a Coldfire MCF5270 for this project. I also have the exact same project running in CodeWarrior 10.2 without this issue.

In CodeWarrior 10.2 when I run debug it connects just fine and downloads.

Capture.PNG.png

I can see the download progress and it takes about 7 seconds.

In CodeWarrior 10.4 when I run debug it also connects just fine but the download looks a bit different and it takes way longer. The progress bar basically jumps right to 100% and then we see "downloading binary to target" where to progress is never indicated. I have to wait about 40 seconds and then it finishes.

Capture2.png

The debug configurations are identical. I cannot find any explanation or setting that can account for this difference. I tried a different debugger and both CodeWarrior versions performed like I describe for 10.2. It seems to be a problem just with the Cyclone Max. Has anyone experienced an issue like this? I updated all the drivers and firmware I could. I am running Windows 7 64-bit.

Thank you.

Labels (1)
0 Kudos
Reply
0 Replies