How can I use the serial-over-USB feature on TWR-5225x?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I use the serial-over-USB feature on TWR-5225x?

Jump to solution
1,761 Views
Kopone
Contributor IV

Hi all,

 

I have a 5225x Tower sitting here and I found in the docs that I can route the UART0 to the OSBDM. I assume that the OSBDM will then transport the serial communication over the USB interface (much like the virtual serial port in the P&E interface).

However I cant find any documentation on how to actually use this.

 

Is there a driver available to make that serial-over-usb port visible on the PC as a regular serial interface so that I can just launch a terminal program?

 

Or is there some proprietary client available like the PE Terminal?

 

It would be great if someone could point me to what I probably overlooked, because that would save me from soldering something to hook up the PC to that 10-pin header on the dev board.

 

Regards,

 Sven

 

Tags (2)
0 Kudos
1 Solution
376 Views
admin
Specialist II

While the hardware hooks supporting serial to USB communications were added, the feature is not currently supported in firmware.  I am not aware of any effort to add the feature at this time.  The souce code is avialable for download and you are free to add the feature if desired. 

View solution in original post

0 Kudos
2 Replies
377 Views
admin
Specialist II

While the hardware hooks supporting serial to USB communications were added, the feature is not currently supported in firmware.  I am not aware of any effort to add the feature at this time.  The souce code is avialable for download and you are free to add the feature if desired. 

0 Kudos
376 Views
Kopone
Contributor IV

Hi Spencer,

I doubt I'll find the time to add this feature myself, but the information is highly appreciated.

Thanks!

 Sven

0 Kudos