FRDM-KL25Z installation failed with USBDM 4.10.6.110.msi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z installation failed with USBDM 4.10.6.110.msi

Jump to solution
789 Views
kai_liu
Senior Contributor I

I downloaded this msi from sourceforge. http://jaist.dl.sourceforge.net/project/usbdm/Version%204.10.6/Software/USBDM_4_10_6_110_Win.msi

While disconnecting OpenSDA of FRDM-KL25Z, I installed the msi file. Then I connect OpenSDA in bootloader mode, upload interface firmware from folder of C:\Program Files\pgo\USBDM 4.10.6.110\FlashImages\MKxx\USBDM_OpenSDA.sx into K20 debug chip. Reconnect, it can enumerate, however it stops at driver installation for "Interface 0 USBDM". because of "The installation wizard can not find necessary software, so the hardware can not be installed properly."

I invoked USBDM TCL Interpreter, enter openbdm command,

% openbdm

Found 1 devices

Failed to open device 0

BDM Open Failed - Device driver may be missing or incorrect

Operation system: Windows XP SP3

I built source code from github. The result is identical. What else should I take care?

0 Kudos
1 Solution
363 Views
pgo
Senior Contributor V
0 Kudos
2 Replies
364 Views
pgo
Senior Contributor V

Hi Kai,

Have you installed the appropriate drivers ?

http://sourceforge.net/projects/usbdm/files/Version%204.10.6/Software/USBDM_Drivers_1_2_0_WinXP_x32....

(or the 64-bit version)

bye

0 Kudos
363 Views
kai_liu
Senior Contributor I

Thanks, pgo,

Installation is success.

0 Kudos