Hi!
The ARM_FlashProgrammer works fine and flashes the KL46Z, but ARM_Gdbserver gives this errror!
For KL25Z works fine.
Thanks,
Sándor
(gdb) load
Loading section .interrupts, size 0xc0 lma 0x0
Loading section .cfmprotect, size 0x10 lma 0x400
Loading section .text, size 0xd01c lma 0x410
Loading section .data, size 0x534 lma 0xd42c
Loading section .romp, size 0x18 lma 0xd960
Start address 0xbf71, load size 54840
qTStatus: Target returns error code 'FF:Closing connection'.
qTStatus: Remote connection closed
Transfer rate: 548 bytes/sec, 1713 bytes/write.
(gdb)
Welcome to USBDM GDB server
Using required USBDM interface S/N = 'USBDM-OPENSDA-13822'
Server created @localhost:1234
=====================================
New client connection from localhost:53321 accepted
Loading register description from device database
BDM Open OK
Sending target description
Sending register description
Reading Registers
Reading Memory[BF70..BF73]
Reading Memory[A58..A59]
Reading Memory[A58..A59]
Erasing flash[0..DBFF] - ignored
Creating flash image
Writing to flash image[0..BF]
Writing to flash image[400..40F]
Writing to flash image[410..BAF]
Writing to flash image[BB0..134F]
Writing to flash image[1350..1ADF]
Writing to flash image[1AE0..226F]
Writing to flash image[2270..29FF]
Writing to flash image[2A00..317F]
Writing to flash image[3180..390F]
Writing to flash image[3910..40AF]
Writing to flash image[40B0..484F]
Writing to flash image[4850..4FEF]
Writing to flash image[4FF0..576F]
Writing to flash image[5770..5F0F]
Writing to flash image[5F10..669F]
Writing to flash image[66A0..6E2F]
Writing to flash image[6E30..75CF]
Writing to flash image[75D0..7D4F]
Writing to flash image[7D50..84EF]
Writing to flash image[84F0..8C7F]
Writing to flash image[8C80..93FF]
Writing to flash image[9400..9B8F]
Writing to flash image[9B90..A31F]
Writing to flash image[A320..AABF]
Writing to flash image[AAC0..B24F]
Writing to flash image[B250..B9CF]
Writing to flash image[B9D0..C15F]
Writing to flash image[C160..C8FF]
Writing to flash image[C900..D0AF]
Writing to flash image[D0B0..D42B]
Writing to flash image[D42C..D95F]
Writing to flash image[D960..D977]
Programming Flash Image failed: Target device does not agree with selected
=====================
Dropped connection
Hi Sandor,
the line
Target device does not agree with selected
indicates the incorrect device is selected.
How are you selecting the device? If you are starting the debugger from Eclipse you need to set the device there. If you are running it stand-alone then you need to select it in the Debugger dialogue.
bye
Hi PGO,
thank you for your answer.
I auto select the device by pressing detect chip button.
Unfortunately I found an other issue with gdbserver.
I flashes the KL46Z by ARM_FlashProgrammer.
Start the gdbserver.
Debug the program.
BUT the debugger able to read only 16k of rams.
In case of KL46Z, ram starts at 0x1fffe000 ends 0x20006000, but the debugger only see up to 0x20002000.
For this small test program I must set the end of stack to 0x20002000 to see the local variables and to be able to step the program correctly.
Yesterday I compiled your latest OPEN_SDA firmware from your git because I've seen your new commits, but the situation is the same.
Anyway, I like very much these tools, because I work on SuSe linux and now I do not need to go to VirtualBox XP's CodeWarrior to develop and debug.
I appreciate your hard work very much!
Thank You,
Sándor
The ram error is found
in arm_devices.xml
<memory id="kinetisL32K_Ram" type="ram">
<memoryRange start="0x1FFFE000" size="16K" />
</memory>
changed to 32k and it work well.
Hi Sandor,
Well spotted about the RAM size - I'll update my files accordingly.
With the first problem I take it you have not installed the Eclipse plugins and you are running the GDB_Server as a stand-alone application?
Can you tell me what Operating System you are using so I can test this situation?
bye
Hi PGO,
I work on SuSe linux 12.3,
bss@bs-s:~> uname -a
Linux bs-s.site 3.7.10-1.16-desktop #1 SMP PREEMPT Fri May 31 20:21:23 UTC 2013 (97c14ba) x86_64 x86_64 x86_64 GNU/Linux
Using stand-alone GDB_Server compiled from you git.
Regards,
Sándor