NXPトレーニングコンテンツ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Training Content

ディスカッション

ソート順:
This session will focus on the wearable reference design for healthcare and explain design challenges, architecture and technical system details. Subject matter experts from Freescale and hardware and software partners will be on hand to demonstrate an i.MX- and Kinetis-based design. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0083
記事全体を表示
As home automation is quickly becoming one of the fastest growing technology markets, interconnected wireless sensors and appliances are an essential building block for creating new and innovative customer experiences. In this session, we will explore just how simple is to add connectivity to home automation applications using Freescale Kinetis wireless MCUs and transceiver solutions, as well as how to benefit from incorporating standard technologies such as ZigBee®, Bluetooth® Smart, or Wi-Fi® into products. We will also discuss system and wireless network architecture best practices and how to overcome major design challenges such as low-power constraints, security concerns and dealing with RF interference. Presented by: Alin Lazar Presented at: FTF 2014 Session ID: FTF-CON-F0410
記事全体を表示
In this hands-on session, the USB features of KL26 will be introduced in-depth, and attendees will learn how easy it is to implement a HID or CDC device with KL26 based on Freescale USB stack. Attendees will then learn that the target board will work as a USB device when connecting to a PC host. Presented at DwF MCU Solutions - Zhengzhou - 31 March 2015 Session ID: APF-IND-T0986
記事全体を表示
Presented by James Huang Presented at MCU and Automotive Solutions, Tianan - 19 March 2015
記事全体を表示
Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015
記事全体を表示
The session will introduce Kinetis MCUs for supporting Thread and embedded platform as well as provide Alljoyn, HomeKit services through MQX.  Presented by James Huang Presented at DwF Taipei - May 7, 2015 Session ID: APF-SHB-T1454
記事全体を表示
The Kinetis Software Development Kit (KSDK) is an extensive set of robust peripheral drivers, communication stacks, middleware and sample applications designed to simplify and accelerate the development in any Kinetis MCU. The addition of Processor Expert technology for software support and board configuration provides ease of use and unmatched flexibility. The Kinetis SDK is free and includes full source code under an open-source permissive license  for all hardware and software abstraction of peripheral drivers. Presented by Denis Shimizu Presented at DwF IoT Multicore Technologies and Enablement Software Solutions - Porto Alegre - 19 March 2015 Session ID: LAT-DES-T1019
記事全体を表示
In this hands-on session, the low-power consumption features and advantages of Freescale KL series MCU will be introduced in-depth, and attendees will learn how to configure the MCU to enter low-power mode, and how to implement the low-power ADC function by practicing on the KL26 target board. Attendees will also learn how to use FreeMASTER (a free tool from Freescale) to monitor and display the running program on the MCU. Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015 Session ID: APF-IND-T1022
記事全体を表示
Internet of Things nodes are using a wide plethora of heterogeneous wireless connectivity protocols such as: IEEE® 802.15.4, Thread, ZigBee®, 6LoWPAN/IPv6, and BLE. By attending this session you will learn which wireless communication protocol is the right solution for their application requirements, while comparing various communication protocols for 2.4 GHz and sub-1 GHz technologies. This session will provide an overview on commonly used wireless technologies and standards for smart homes and which Freescale microcontroller families are best suited for connected appliance, sensor device or hub product idea. Presented by Antonio Concio Presented at DwF Istanbul/Ankara - May 12/14, 2015 Session ID: EUF-IND-T1462
記事全体を表示
Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015
記事全体を表示
This session will give an overview on Freescale ARM microcontrollers and product series roadmap for Kinetis MCUs based on ARM® Cortex®-M4 / M+ and i.MX applications processors based on Cortex-A8 and Cortex-A9. The session will also introduce Freescale segment focus on Kinetis MCUs, such as KM, KM and KV series.  Presented by James Huang Presented at DwF Taipei - May 7, 2015 Session ID: APF-IND-T1453
記事全体を表示
Design, Software and Services Accelerating Firmware Development of Kinetis MCUs by using the New Peripheral Drives, Stacks and Middleware of Kinetis SDK Hands-On Workshop: MQX™ RTOS and Kinetis Software Development Kit (SDK) Integration   Smart Industry Hands-On Workshop: Introduction to the Development of Embedded Systems with Asymmetric Multicore Approach Networking Applications with Yocto Project™ Operation Presenting the New QorIQ LS1 MPUs for IoT, M2M
記事全体を表示
Smart Home and Buildings Wi-Fi Module from Freescale and QualComm Smart Networks K22FSH Development
記事全体を表示
This hands-on session will detail how to build portable and diagnostic devices using the Kinetis ARM® Cortex®-M0 and Cortex-M4 products from Freescale. Special attention will be paid to the integration of sensors and Bluetooth® low energy. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0197
記事全体を表示
Freescale is the best positioned silicon maker for the Internet of Tomorrow. This session is all about how Freescale sees the mechanics of the IOT. Attend this session and see what runs under the hood! Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-IND-T1463
記事全体を表示
ARM Processors i.MX 2014 Archives Kinetis Power Architecture Processors QorIQ Analog and Power Management RF Sensors 2014 Archives Wireless Connectivity 2014 Archives Medical and Healthcare 2014 Archives Additional Courses Material
記事全体を表示
Design, Software and Services Bootloader Solution for Kinetis MCUs Insight and Innovation Total Sensor Hub and Fusion Solution Smart Home and Buildings Share Design Experience Using i.MX Applications Processors based on ARM® Cortex®-A7 and Cortex-A9 Cores Freescale IoT Solutions - Taipei Freescale Wireless Charging Technology Smart Industry Freescale ARM® Microcontroller Overview Analog Product Introduction Including PMIC, SBC and PowerPC Smart Networks Wireless MCU Product Update QorIQ WLAN Wave-2 EAP Solution Update
記事全体を表示
Presented at DwF Kinetis MCUs Based on ARM® Technology - Jinan - 22 April 2015
記事全体を表示
Join this hands-on workshop to learn about the newest Kinetis software development tools (e.g., Kinetis Design Studio IDE, Processor Expert, SDK) and work with a Freedom platform to kick-start your next application development based on Kinetis MCUs. During this class we will walk through hands-on labs showing you how to create and debug a project for the Freedom development platform for Kinetis MCUs. It will dive into the internals of the Kinetis SDK libraries exploring board configurations, clock management, the hardware abstraction layer, peripheral driver usage, the USB stack, RTOS integration and more. Presented by Antonio Concio & Lorenzo Daniele Presented at DwF Istanbul - May 12, 2015 Session ID: EUF-IND-T1475
記事全体を表示
Learn about Freescale's latest Kinetis and i.MX devices plus view the roadmap offerings. Presented by Dong Sun Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015 Session ID: APF-INS-T1013
記事全体を表示