恩智浦培训内容

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP Training Content

讨论

排序依据:
Lecture including a live demo, showing how to develop multimedia application for i.MX applications processors, taking advantages of the hardware multimedia accelerators of the i.MX SoC.  Presented by Daniele DallAcqua Presented at DwF Istanbul - May 12, 2015 Session ID: EUF-DES-T1474
查看全文
The i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) is a NXP development platform based on Cortex A-35 + Cortex-M4 cores. Built with high-level integration to support graphics, video, image processing, audio, and voice functions, the i.MX 8X processor family is ideal for safety-certifiable and efficient performance requirements. This tutorial shows how to enable the Cortex-M4 using the MCUXpresso SDK package and loading the binary from the network. NOTE: It is also possible to load the Cortex-M4 image from the SCFW using the imx-mkimage utility. Please see next blog posts for this tutorial. Setting up the machine NOTE: This shows the procedure for a Linux environment. For the Windows OS, please see the Getting Started documentation on the SDK package. Install cmake on the host machine: $ sudo apt-get install cmake Download the armgcc toolchain from here :https://launchpad.net/gcc-arm-embedded/5.0/5-2016-q2-update/+download/gcc-arm-none-eabi-5_4-2016q2-20160622-linux.tar.bz2  and export the location as ARMGCC_DIR: $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-5_4-2016q2/ NOTE: The ARMGCC_DIR variable needs to be exported on the terminal used for compilation. To setup the TFTP server on the host machine, follow the first two sections on this blog post https://imxdev.gitlab.io/tutorial/How_to_boot_Kernel_and_File_System_from_the_network/ (Configuring your Host PC for TFTP and Configuring your Host PC for NFS). Downloading the SDKPermalink Download the MCUXpresso SDK following these steps: Click on “Select Development Board”; Select MEK-MIMX8QX under “Select a Device, Board, or Kit” and click on “Build MCUXpresso SDK” on the right; Select “Host OS” as Linux and “Toolchain/IDE” as GCC ARM Embedded; Add “FreeRTOS” and all the wanted Middleware and hit “Request Build”; Wait for the SDK to build and download the package. Building the image All demos and code examples available on the SDK package are located in the directory <<SDK_dir>>/boards/mekmimx8qx/. This tutorial shows how to build and flash the hello_world demo but similar procedures can be applied for any example (demo, driver, multicore, etc) on the SDK. To build the demo, enter the armgcc folder under the demo directory and make sure that the ARMGCC_DIR variable is set correctly. $ cd ~/SDK_2.3.0_MEK-MIMX8QX/boards/mekmimx8qx/demo_apps/hello_world/armgcc $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-5_4-2016q2/ Run the build_release.sh script to build the code. $ ./build_release.sh NOTE: If needed, give the script execution permission by running chmod +x build_release.sh. This generates the M4 binary (hello_world.bin) under the release folder. Copy this image to the /tftpboot/ directory on the host PC. NOTE: This procedure shows how to build the M4 image that runs on TCM. To run the image from DDR, use the build_ddr_release.sh script to build the binary under the ddr_release folder. Flashing the image Open two serial consoles, one for /dev/ttyUSB0 for Cortex-A35 to boot Linux, and one for /dev/ttyUSB1 for Cortex-M4 to boot the SDK image. On the A35 console, with a SD Card with U-Boot, stop the booting process and enter the following commands to load the M4 binary to TCM: => dhcp => setenv serverip <ip_from_host_pc> => tftp 0x88000000 hello_world.bin => dcache flush => bootaux 0x88000000 Then the M4 core will load the image to the /dev/ttyUSB1 console.    
查看全文
The i.MX 6UltraLite EVK kernel release includes the parallel camera OV5640 support by default. However, depending on the base board revision, this camera might require the SCH700-27820 adapter below: Camera Adapter According to the following image, the FX12B-40P-0.4SV connector layout was changed in the RevC, giving the possibility to use the OV5640 directly:   Rev B in the left and Rev C in the right, which does not need the adapter So, if you are using a base board older than Rev C, plug in the camera with the adapter and connect the other end of the adapter to the board.   In order to use the parallel OV5640 camera, it’s necessary to set up the environment variable below on U-Boot, independent of the base board revision: => setenv fdt_file ‘imx6ul-14x14-evk-csi.dtb’ => saveenv Follow the GStreamer pipeline example to test the camera connection: $ gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,width=640,height=480 ! autovideosink   This test was done using the kernel BSP release 5.10.35v.  
查看全文
This section describes some advanced topics and tips to get high experiences in camera use cases in the i.MX 8 boards The i.MX 8QM MEK includes the use of the dual MIPI-CSI interfaces and two MX8XMIPI4CAM2 in combination with eight MCIMXCAMERA1MP daughter cards connected to them. For this, change the DTB file to fsl-imx8qm-mek-8cam.dtb and boot the board. Figure 1. Show i.MX 8QM MEK 8 cameras example.   Multiple cameras output In order to use more than one camera at the same time displayed in the same monitor output, boot the board and enter with the following command line to get the cameras ids: $ v4l2-ctl --list-devices It will result in something similar to the image below: Figure 2. v4l2-ctl results According to the image, mxc-isi found and set four cameras to /dev/video0, video1, video2, and video3. So we can build the GStreamer pipeline below changing it as required: $ gst-launch-1.0 -v imxcompositor_g2d name=comp \ sink_0::xpos=0 sink_0::ypos=0 sink_0::width=640 sink_0::height=480 \ sink_1::xpos=0 sink_1::ypos=480 sink_1::width=640 sink_1::height=480 \ sink_2::xpos=640 sink_2::ypos=0 sink_2::width=640 sink_2::height=480 \ sink_3::xpos=640 sink_3::ypos=480 sink_3::width=640 sink_3::height=480 \ ! video/x-raw,format=RGB16 ! waylandsink \ v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! comp.sink_0 \ v4l2src device=/dev/video1 ! video/x-raw,width=640,height=480 ! comp.sink_1 \ v4l2src device=/dev/video2 ! video/x-raw,width=640,height=480 ! comp.sink_2 \ v4l2src device=/dev/video3 ! video/x-raw,width=640,height=480 ! comp.sink_3   This pipeline enables the user to set up more than one camera to the same screen using the imxcompositor_g2d for it. This is the unique solution available to create an interface over Weston/Wayland interface, i.e., in i.MX 8 devices we need to use GPU to create interfaces GUI. This pipeline results in the image below: Figure 3. GStreamer 4 cameras output It is just an example and you are encouraged to change it for other camera use cases, such as the eight cameras supported by the i.MX 8QM MEK.          
查看全文
This session will focus on the wearable reference design for healthcare and explain design challenges, architecture and technical system details. Subject matter experts from Freescale and hardware and software partners will be on hand to demonstrate an i.MX- and Kinetis-based design. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0083
查看全文
As home automation is quickly becoming one of the fastest growing technology markets, interconnected wireless sensors and appliances are an essential building block for creating new and innovative customer experiences. In this session, we will explore just how simple is to add connectivity to home automation applications using Freescale Kinetis wireless MCUs and transceiver solutions, as well as how to benefit from incorporating standard technologies such as ZigBee®, Bluetooth® Smart, or Wi-Fi® into products. We will also discuss system and wireless network architecture best practices and how to overcome major design challenges such as low-power constraints, security concerns and dealing with RF interference. Presented by: Alin Lazar Presented at: FTF 2014 Session ID: FTF-CON-F0410
查看全文
This session will show how to obtain i.MX technical information from Freescale's website and also give an overview on i.MX 6 series SoC features, including IPU, VPU, GPU, and corresponding i.MX 6 series hardware design reference boards. The session will also show how to use Android® BSP for i.MX 6 series processors KK4.4.2_1.0.0-ga, i.MX 6 series for Linux® BSP fsl-yocto-3.10.17_1.0.0-ga and manufacturing tools. At the end of this session, we will do a few case studies on i.MX 6 series, i.e. multiple camera capturing, dashboard demo, multi-panel display. Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015 Session ID: APF-DES-T1021
查看全文
Presented by James Huang Presented at MCU and Automotive Solutions, Tianan - 19 March 2015
查看全文
Presented by Gemotech Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015
查看全文
The session will introduce Kinetis MCUs for supporting Thread and embedded platform as well as provide Alljoyn, HomeKit services through MQX.  Presented by James Huang Presented at DwF Taipei - May 7, 2015 Session ID: APF-SHB-T1454
查看全文
Learn practical methods to integrate video and graphical elements together in your user interface that runs on the i.MX 6 series. The session starts with an introduction of the i.MX 6 series video and graphics hardware components, along with their Linux® OS software libraries. It will then show simple methods to create portable user interface applications, supported by several useful software code examples. Presented by: Daniele Dall'acqua Presented at: FTF 2014 Session ID: FTF-CON-F0223
查看全文
This session will introduce i.MX 6 series hardware design reference board and will walk through the i.MX 6 series SDP schematic. The session will also introduce hardware design consideration including the hardware checking list to facilitate the hardware design and development. Additionally i.MX6D/Q/DL/Solo power design and how to use DDR calibration will be covered. At the end of session, will share the experience of i.MX 6 hardware bring up. Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015 Session ID: APF-DES-T1023
查看全文
This session will give an overview on Freescale ARM microcontrollers and product series roadmap for Kinetis MCUs based on ARM® Cortex®-M4 / M+ and i.MX applications processors based on Cortex-A8 and Cortex-A9. The session will also introduce Freescale segment focus on Kinetis MCUs, such as KM, KM and KV series.  Presented by James Huang Presented at DwF Taipei - May 7, 2015 Session ID: APF-IND-T1453
查看全文
Learn how an image flows through an i.MX 6 series or i.MX5x applications processor from the sensor, through the image processing unit (IPU), all the way to the display. Learn to set up and control the image path, as well as where the BSP and Uboot must be touched to effect changes. This session will include an instructor-led demonstration based on i.MX 6 series applications processors and homework. Presented by: Oliver Brown Presented at: FTF 2014 Session ID: FTF-CON-F0119
查看全文
Freescale is the best positioned silicon maker for the Internet of Tomorrow. This session is all about how Freescale sees the mechanics of the IOT. Attend this session and see what runs under the hood! Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-IND-T1463
查看全文
ARM Processors i.MX 2014 Archives Kinetis Power Architecture Processors QorIQ Analog and Power Management RF Sensors 2014 Archives Wireless Connectivity 2014 Archives Medical and Healthcare 2014 Archives Additional Courses Material
查看全文
Design, Software and Services Bootloader Solution for Kinetis MCUs Insight and Innovation Total Sensor Hub and Fusion Solution Smart Home and Buildings Share Design Experience Using i.MX Applications Processors based on ARM® Cortex®-A7 and Cortex-A9 Cores Freescale IoT Solutions - Taipei Freescale Wireless Charging Technology Smart Industry Freescale ARM® Microcontroller Overview Analog Product Introduction Including PMIC, SBC and PowerPC Smart Networks Wireless MCU Product Update QorIQ WLAN Wave-2 EAP Solution Update
查看全文
Learn about Freescale's latest Kinetis and i.MX devices plus view the roadmap offerings. Presented by Dong Sun Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015 Session ID: APF-INS-T1013
查看全文
Presented by Embedsky Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015
查看全文
This session will explain how the IoT will change healthcare. Subject matter experts from Freescale and software partners will discuss the One Box reference platform and how it can be used to enable the IoT for healthcare applications. Special attention will be paid to hardware design, communication protocols and the security structure. Presented by: David Niewolny Presented at: FTF 2014 Session ID: FTF-HCR-F0195
查看全文