RADAR Toolbox for S32R (SPT) License Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RADAR Toolbox for S32R (SPT) License Failure

1,295 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

My customer reported following issue:

I get an error while using the add_mex(1i,1i,0,0) function to verify the license.

My Host ID: 70-B5-E8-81-D0-8A.

ERROR:
SPTToolbox: License error.
SPTToolbox: License error.
错误使用 link_mex
MEX 文件 'C:\Users\Administrator\AppData\Roaming\MathWorks\MATLAB
Add-Ons\Toolboxes\NXP_RADAR_Toolbox_for_S32R\mex\sim\sim_spt20_mex.mexw64' 无效: 动态链接库(DLL)初始化例程失败。

Screenshot_2.jpg

Screenshot_1.jpg

  

Thanks,

Peter

0 Kudos
Reply
1 Reply

1,286 Views
iulianbulancea
NXP Employee
NXP Employee

Hello,

 

As a Host ID, instead of Ethernet Address can you use Disk Serial Number? You can find the Disk Serial Number by calling in the command line vol C:.

 

Kind regards,

Iulian Bulancea

0 Kudos
Reply