Hi
I was simulating the simulink file of V/F scalar control(M5_2018.R1) which is available in https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Module-7-Torque-Control/m-p/736921.
When I gave 200 rad/sec as the commanded speed and simulated, the motor phase current is around 6 A (approx) , where as the load torque is zero.
As per the data sheet of Linix motor 45ZWN24-40, the max current is 2.3 A.
Could you please check and confirm the above query?
Thanks in advance.