How to use radarSDK ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use radarSDK ?

1,904 Views
pingfang
Contributor III

Hello,

How to use radarSDK as soon as possible?

Can you give me some suggestions?

Thank you very much!

Regards,

Ping Fang

0 Kudos
Reply
3 Replies

1,452 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Ping Fang, 

We were told that the SDK will become available for download on this page: S32R Radar Microcontroller - S32R27|NXP 

I checked the page but it is still not there. I'll try to check internally to see what was the cause of delays.

Thank you for your interest

Daniel

0 Kudos
Reply

1,452 Views
pingfang
Contributor III

Hi Daniel,

Thank you for your reply.

Now, I have the radarSDK .

Can you tell me how to use it as soon as possible?

0 Kudos
Reply

1,452 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi pingfang‌,

It depends on your plans of using it.

If you wish to simulate the RADAR processing then please refer to https://community.nxp.com/message/970502 

If you wish to start the development for the board with C-source, then you should refer to the SDK release notes for the appropriate environment setup and once you install the correct version of the S32 Design Studio then you will be able to run the examples from the SDK or go ahead with your own development starting from those examples.

Hope this helps!

Daniel 

0 Kudos
Reply