NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
Trusted Platform Modules (TPMs) are standards based hardware roots of trust with protected key storage. This session covers how QorIQ Trust Architecture primitives can be used as Soft TPM, thereby reducing BOM cost by eliminating a discrete TPM chip.
View full article
Wayland and Weston are gaining popularity as Window Manager and Compositor on Linux, and they are part of our reference board support package (BSP). This lesson dives deep into the setup of Wayland/Weston on custom BSPs, enabling xWayland, and successful configuration of advanced multi-display and multi-input setups on i.MX applications processors.
View full article
Solid state RF energy provides cooking appliance OEMs the opportunity to create differentiated cooking appliances. When combined with emerging food services, these appliances can enable greater levels of consumer convenience while delivering consistent cooking results. This session will cover the underlying basics of how solid state RF cooking is performed, its benefits, and how it can be combined in an IoT appliance to deliver even further differentiation. Watch Video Presentation
View full article
This session will cover the different vision processing capabilities of the S32V234 automotive vision processor with a focus on the Image Sensor Processor (ISP). The presentation will demonstrate how the cost of a vision system can be cut down by using the ISP to accept raw camera input data and to process it using algorithms like debayering, white balancing, format conversion, HDR and de-noising. The aim of the session is to give an introduction to camera processing, to present the architecture of the ISP and to demonstrate how it can be programmed using a visual tool developed by NXP.
View full article
Building on top of 11 years of usage within data centers, Xen Hypervisor is uniquely placed to support a new range of use cases for embedded solutions. In particular, its isolation and security features, flexible virtualization modes and architecture, driver disaggregation, and strong ARM support make it a perfect fit for embedded applications. Artem Mygaiev, GlobalLogic’s Embedded Practice Head, will explore the virtualization nuances and challenges of using Xen Hypervisor for embedded applications through the demonstration of his own company’s journey in developing a platform that leverages Xen for virtual network equipment, IoT, automotive, and other embedded use cases.
View full article
This session will present the structure of NXP Yocto layers and mechanism of software delivery. Various architectures (ARM®v7, ARM®v8 and PPC) can be supported, the common software components can be shared by different products (i.MX and QorIQ processors) via the unified NXP Yocto layer which manages the free software and maintained by Yocto community. The commercial software can be delivered via separated layers, QorIQ LS2 SDK is using the mechanism for commercial software delivery, e.g. nsp, openflow, ssp and tcpoffload. The session also introduces how to create Yocto layer for customization changes and commercial products. Watch Video Presentation
View full article
Explore the NXP wearable and fitness product roadmap and solutions platform. Watch Video Presentation
View full article
A modern car is more than just transport, it provides comfortable heating and cooling, navigation systems, entertainment systems, and a lot of data about the car's health and performance. Including how well you are conserving fuel or when to seek service. All of this is a challenge to present to the driver and passengers, without distraction to driving, under all conditions from bright daylight to the dark of night, in any temperature. We talk about both Liquid Crystal Display (LCD) and Light Emitting Diode (LED) component solutions that keep your dashboard simple, readable, and helpful. Watch Video Presentation
View full article
There are many variables to consider when implementing and integrating solid state RF power into a cooking appliance. Cavity size and shape, RF feed type, power, thermals, and configuration all factor into design consideration. This session will cover key consideration and methods of simulating to achieve better system design. Watch Video Presentation
View full article
This hands-on workshop will help you get started with our latest MAC57D5xx processor for instrument cluster and human machine interfaces together with the recent release of MQX. Practical use cases will be demonstrated and exercised during this hands-on workshop session.
View full article
This presentation will cover the Hardware Security Module (HSM) and how to use the software kits NXP offers, the HSM Security Firmware and HSM Software Development Kit. We will also cover other security features of the device offered by modules like PASS or TDM and their configuration. Watch Video Presentation
View full article
The need to ensure electrical power availability is increasing. Batteries are spreading into automotive, electrical storage systems and uninterruptible power supplies. This session will present the benefits of NXP Battery Management Solutions for multiple battery architectures. Watch Video Presentation
View full article
Detailed training session on developing with the LPCXpresso Ecosystem, showing the main features of the tools, from project import/creation, multi-core debug and power optimization. The LPCXpresso boards and IDE toolchain will be used with the latest version of LPCOpen peripheral driver examples. We will cover some cool new features including trace and power analysis.
View full article
Deep dive into the vision processing architecture of the i.MX 8 family. Learn how to access the advanced processing features, the vision SDK, and the vision-based applications enabled by the i.MX 8 processor. This class provides an introduction to understanding the unique way in which machine vision is handled by i.MX 8. It forms a basic introduction class that is a precursor to the more advanced "Call Your Shot!" pool table demo class. Watch Video Presentation
View full article
NXP is one of the pioneers in bringing helping bring multicore solutions to the aviation industry and helping customers navigate the certification requirements. This session will cover the roadmap and status of current certification activities, challenges for 2016 we are addressing for both PPC and ARM devices.
View full article
As the Smart Home starts to gather momentum, a number of competing Wireless Communication standards are fighting for dominance. With ZigBee® now becoming dominant in the low-power networking market, there is no surprise that two new low power technology Thread and Bluetooth® Low Energy with the new Mesh capability are both trying to enter this market to get a piece of the cake. Moreover competing IoT platforms from the Thread Group (Google/Nest), Allseen Alliance (Qualcomm), Apple's Homekit, the Open Interconnect Consortium (Intel) and many others are creating even more confusion. So in this confusing array of Wireless Communication standards and Iot platforms, what are the main features of each and what does it means for NXP? This session will provide an overview of these Wireless connectivity standards and IoT platforms, their capabilities, and their implication for NXP IoT. Watch Video Presentation
View full article
Learn how NXP's Motor Control reference design and control libraries, built on the Kinetis V portfolio, can help you beat deadlines, improve your time to market, and achieve better motor performance. In this hands-on class you will learn how to use NXP's complimentary reference designs and control libraries to get to market quicker with better designs.
View full article
We'll walk through the available tools and middleware for rapid development of graphics applications across multiple operating systems, and look at advanced profiling and debugging of the rendering subsystems on the i.MX 6 and i.MX 8 applications processors.
View full article
This hands-on class will walk you through developing two separate applications. First, learn how to leverage a FlexIO driver to add some autonomous monitoring and reaction to sensor data. Secondly, learn how to create a complex parallel interface (TFT driver).
View full article
This session will provide tips that will help speed up silicon bring up of the QorIQ LS1043A processor.
View full article