MHW-N1979 Designing NFMI-based Wireless Earphones with Hearables Application Development Kit 1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MHW-N1979 Designing NFMI-based Wireless Earphones with Hearables Application Development Kit 1.0

MHW-N1979 Designing NFMI-based Wireless Earphones with Hearables Application Development Kit 1.0

About a decade ago, NXP introduced its first generation Near Field Magnetic Induction (NFMI) radio, to help connecting hearing impaired persons with the digital world. Today, besides medical applications, NFMI is also being used in consumer devices to reduce power consumption and not be affected by body tissue absorption. NXP NFMI allows for hearable and wearable devices that can fit inside an ear canal or be worn on the body. Power levels are low enough to run for a week on a single ZnAir battery. Applications include truly wireless earbuds, implantable electronics, body area networks, under water communication devices, and many other low power.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎05-25-2016 09:52 AM
更新者: