Hello~
I use lx2160ardb board.
Why are u-boot's printenv and linux's fw_printenv default values different?
How do i set if i want to use the same default value?
已解决! 转到解答。
hi~ Thank you for your help.
but, i solved my problem myself.
u-boot printenv & linux fw_printenv default value is different.
- Linux fw_printenv(ex. bootdelay=2) is downloaded binary for url.
- U-boot printenv is compiled with my configuration(ex. bootdelay=10).
So, default value is different.
And i tried to compile u-boot/tools/env/ directory, then fw_printenv that compiled has same default env as u-boot printenv tool.
Hello songhee yun,
After creating configuration file /etc/fw_env.config as the following, I execute command "fw_printenv" to get u-boot environment parameters as the attachment, I compared this file with the one generated by u-boot pri command, they are same.
# cat /etc/fw_env.config
/dev/mtd0 0x500000 0x2000 0x20000
Please make sure you get u-boot environment parameters from the same flash bank.
Thanks,
Yiping
Hello yipingwang
I uses sd card(DIP SW1 1111->1000) and CONFIG_SYS_MMC_ENV_DEV 0 -> 1
I configure fw_env.conf already. and i tested 2 cases.
/dev/mmcblk0 0x500000 0x2000
First, i tried '# env default -f -a' at u-boot command line.
Second, i tried 'dd if=/dev/null of=/dev/mmcblk0 bs=1 skip=0x500000 seek=0x500000 count=20' after linux booting.
And that cases results are different.
hi~ Thank you for your help.
but, i solved my problem myself.
u-boot printenv & linux fw_printenv default value is different.
- Linux fw_printenv(ex. bootdelay=2) is downloaded binary for url.
- U-boot printenv is compiled with my configuration(ex. bootdelay=10).
So, default value is different.
And i tried to compile u-boot/tools/env/ directory, then fw_printenv that compiled has same default env as u-boot printenv tool.