Hello guys
After flashing my device over the mass storage it doesnt show up on the pc.
I also have an evalboard but there is no Problem with the connection and the Vcom on the desktop.
Do I have to install another file to get it running.
Because I dont think that it is a Hardware Problem.
-> Windows 10
Yurs faithfully
Raphael
Hello fangfang
The chapter 5.3 (4.3) does not help me in the slightest because I am already able to Flash the PN7462.
The only Problem is that i can´t see the vCom on the PC after the flashing the two files "Flash & EEPROM" just as the evalboard.
I already checked the voltages and the Connections compared to the evalboard PNEV7462C.
I am using the PN7462AUHN and the following files:
….03_04_00_Flash.bin
….28_00_00_EEPROM.bin