MK12DN512的复位管脚电压

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK12DN512的复位管脚电压

639 Views
zcm221
Contributor I

你好,最近遇到一个奇怪的问题,软硬件均无问题的情况下,连续通过JLINK给3块板下载程序,下载后均无法运行,RESET管脚均变为1.5V左右(原均为3.3V),以前都是好的电路板和调试通过的程序,是什么问题?谢谢

原以为JLINK有问题,又买了一个新的(非正版),但问题依旧,用一块老电路板试了试,程序一下载,电路板RESET管脚立即变成约1.6V, 现在都不敢再下载调试了

芯片MK12DN512VLH5,已用了3-4年了,开发环境CW

0 Kudos
1 Reply

580 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

你能拿示波器观察一下reset脚的波形吗。我怀疑你可能会看到锯齿状的波形。如果是这样的话,你的芯片被软件锁住了(lock)。你可以用jlink解锁(unlock)。

Regards,
Jing

0 Kudos